Data Fields
ClockP_Struct Union Reference

ClockP structure. More...

#include <ClockP.h>

Data Fields

uint32_t dummy
 
uint8_t data [(68)]
 

Detailed Description

ClockP structure.

Opaque structure that should be large enough to hold any of the RTOS specific ClockP objects.

Field Documentation

§ dummy

uint32_t ClockP_Struct::dummy

Align object

§ data

uint8_t ClockP_Struct::data[(68)]

The documentation for this union was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale