Data Fields
XMEM_Attrs Struct Reference

XMEM attributes. More...

#include <XMEMWFF3.h>

Collaboration diagram for XMEM_Attrs:
Collaboration graph
[legend]

Data Fields

FlashType flashType
 

Detailed Description

XMEM attributes.

The address of an XMEM_Attrs structure is passed to XMEMWFF3_getAttrs().

See also
XMEMWFF3_getAttrs()

Field Documentation

§ flashType

FlashType XMEM_Attrs::flashType

Configuration for the specific flash memory hardware


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale