Data Fields
UART2WFF3_Object Struct Reference

UART2WFF3 Object. More...

#include <UART2WFF3.h>

Collaboration diagram for UART2WFF3_Object:
Collaboration graph
[legend]

Data Fields

UART2_BASE_OBJECT Power_NotifyObj preNotify
 
Power_NotifyObj postNotify
 
uint32_t * dmaTxDestAddr
 
uint32_t * dmaRxSrcAddr
 

Detailed Description

UART2WFF3 Object.

The application must not access any member variables of this structure!

Field Documentation

§ preNotify

UART2_BASE_OBJECT Power_NotifyObj UART2WFF3_Object::preNotify

For configuring IO pins before entering sleep

§ postNotify

Power_NotifyObj UART2WFF3_Object::postNotify

For configuring IO pins after returning from sleep

§ dmaTxDestAddr

uint32_t* UART2WFF3_Object::dmaTxDestAddr

§ dmaRxSrcAddr

uint32_t* UART2WFF3_Object::dmaRxSrcAddr

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale