Data Fields
StructRingBuf_Object Struct Reference

#include <StructRingBuf.h>

Data Fields

uint8_t * buffer
 
size_t length
 
size_t count
 
size_t head
 
size_t tail
 
size_t maxCount
 
size_t structSize
 

Field Documentation

§ buffer

uint8_t* StructRingBuf_Object::buffer

§ length

size_t StructRingBuf_Object::length

§ count

size_t StructRingBuf_Object::count

§ head

size_t StructRingBuf_Object::head

§ tail

size_t StructRingBuf_Object::tail

§ maxCount

size_t StructRingBuf_Object::maxCount

§ structSize

size_t StructRingBuf_Object::structSize

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale