Data Fields
SDWFF3_Param Struct Reference

#include <SDWFF3.h>

Data Fields

void * SDWFF3CallbackFxn
 
uint32_t minDmaTransferSize
 

Field Documentation

§ SDWFF3CallbackFxn

void* SDWFF3_Param::SDWFF3CallbackFxn

Application call-back function

§ minDmaTransferSize

uint32_t SDWFF3_Param::minDmaTransferSize

Minimum transfer size for DMA based transfer


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale