Data Fields
PowerWFF3_Config Struct Reference

Global configuration structure. More...

#include <PowerWFF3.h>

Data Fields

Power_PolicyInitFxn policyInitFxn
 The Power Policy's initialization function. More...
 
Power_PolicyFxn policyFxn
 The Power Policy function. More...
 

Detailed Description

Global configuration structure.

Field Documentation

§ policyInitFxn

Power_PolicyInitFxn PowerWFF3_Config::policyInitFxn

The Power Policy's initialization function.

If the policy does not have an initialization function, 'NULL' should be specified.

§ policyFxn

Power_PolicyFxn PowerWFF3_Config::policyFxn

The Power Policy function.

When enabled, this function is invoked in the idle loop, to opportunistically select and activate sleep states.

Two reference policies are provided:

PowerWFF3_doWFI() - a simple policy that invokes CPU wait for interrupt (WFI)

PowerWFF3_sleepPolicy() - an aggressive policy that considers constraints, time until next scheduled work, and SLEEP state latencies, and optionally puts the device into the SLEEP state, the IDLE state, or as a minimum, WFI.

Custom policies can be written, and specified via this function pointer.

In addition to this static selection, the Power Policy can be dynamically changed at runtime, via the Power_setPolicy() API.

If not NULL, the policy function will be invoked once for each pass of the idle loop.

The power policy can be dynamically enabled and disabled at runtime, via the Power_enablePolicy() and Power_disablePolicy() functions, respectively.


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale