Data Fields
PWMTimerWFF3_HwAttrs Struct Reference

PWMTimerWFF3 Hardware attributes. More...

#include <PWMTimerWFF3.h>

Data Fields

uint8_t gpTimerInstance
 
uint16_t preScalerDivision
 

Detailed Description

PWMTimerWFF3 Hardware attributes.

These fields are used by the driver to set up the underlying GPTimer driver statically.

Field Documentation

§ gpTimerInstance

uint8_t PWMTimerWFF3_HwAttrs::gpTimerInstance

GPTimer unit index (0, 1)

§ preScalerDivision

uint16_t PWMTimerWFF3_HwAttrs::preScalerDivision

GPTimer prescaler divider


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale