Data Fields
LogSinkBuf_Rec Struct Reference

#include <LogSinkBuf.h>

Data Fields

uint32_t serial
 
uint32_t timestampHigh
 
uint32_t timestampLow
 
LogSinkBuf_RecordType type
 
uint32_t data [(5)]
 

Field Documentation

§ serial

uint32_t LogSinkBuf_Rec::serial

§ timestampHigh

uint32_t LogSinkBuf_Rec::timestampHigh

§ timestampLow

uint32_t LogSinkBuf_Rec::timestampLow

§ type

LogSinkBuf_RecordType LogSinkBuf_Rec::type

§ data

uint32_t LogSinkBuf_Rec::data[(5)]

The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale