![]() |
![]() |
GPTimerWFF3 channel dependent pin configuration struct. More...
#include <GPTimerWFF3.h>
Data Fields | |
| uint8_t | pin |
| uint8_t | pinMux |
| uint8_t | nPin |
| uint8_t | nPinMux |
GPTimerWFF3 channel dependent pin configuration struct.
GPTimer struct used by the GPTimerWFF3_HWAttrs.
| uint8_t GPTimerWFF3_ChannelConf::pin |
Channel pin
| uint8_t GPTimerWFF3_ChannelConf::pinMux |
Channel pin mux
| uint8_t GPTimerWFF3_ChannelConf::nPin |
Complementary channel pin
| uint8_t GPTimerWFF3_ChannelConf::nPinMux |
Complementary channel pin mux