Data Fields
FlashRegister Struct Reference

Flash register structure for address-data pairs. More...

#include <XMEMWFF3.h>

Data Fields

uint32_t address
 
uint32_t data
 

Detailed Description

Flash register structure for address-data pairs.

Structure used to define register address and data value pairs for STIG operations in flash memory.

Field Documentation

§ address

uint32_t FlashRegister::address

Register address for flash operation

§ data

uint32_t FlashRegister::data

Data value to write to or read from the register


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale