Data Fields
FlashPollingCfg Struct Reference

Flash polling configuration structure. More...

#include <XMEMWFF3.h>

Data Fields

uint32_t NumOfIteration
 
uint32_t command
 
uint32_t timeOut
 
uint32_t polarity
 
uint32_t mask
 

Detailed Description

Flash polling configuration structure.

Structure containing parameters for polling flash status during operations.

Field Documentation

§ NumOfIteration

uint32_t FlashPollingCfg::NumOfIteration

Maximum number of polling iterations

§ command

uint32_t FlashPollingCfg::command

Command to execute for polling

§ timeOut

uint32_t FlashPollingCfg::timeOut

Timeout value for polling operation

§ polarity

uint32_t FlashPollingCfg::polarity

Expected polarity of status bit

§ mask

uint32_t FlashPollingCfg::mask

Bit mask for status checking


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale