Data Fields
ADCWFF3_Object Struct Reference

ADCWFF3 Object. More...

#include <ADCWFF3.h>

Collaboration diagram for ADCWFF3_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
Power_NotifyObj postNotify
 

Detailed Description

ADCWFF3 Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool ADCWFF3_Object::isOpen

Flag if the instance is in use

§ postNotify

Power_NotifyObj ADCWFF3_Object::postNotify

For reconfiguration after Sleep


The documentation for this struct was generated from the following file:
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale