File List
Here is a list of all files with brief descriptions:
 ADC.hAnalog to Digital Conversion (ADC) Input Driver
 ADCWFF3.hADC driver implementation for the ADC peripheral on Wi-Fi F3 devices
 AnsiColor.h
 Board.hPortable board-specific symbols
 Button.hButton driver
 ClockP.hClock interface for the RTOS Porting Interface
 CommonResourceXXF3.hShared resources to arbitrate access to the HSM, CAN, and APU
 DebugP.hDebug support
 Display.hGeneric interface for text output
 DisplayHost.hDisplay driver for printf-like output
 DisplayUart2.hDisplay.h implementation for UART output
 DMAWFF3.hDMAWFF3 driver implementation
 Driver_Init.h
 EventP.hEvent Group support
 FlashWFF3.h
 GPIO.hGeneral Purpose I/O driver interface
 GPIOWFF3.hGPIO driver implementation for WiFi F3 devices
 GPTimerWFF3.hGPTimer driver implementation for Wi-Fi F3 devices
 HSMResourceXXF3.hShared resources to arbitrate access to the HSM
 hw_cpu_dwt.h
 hw_cpu_itm.h
 hw_cpu_scs.h
 hw_cpu_tpiu.h
 HwiP.hHardware Interrupt module for the RTOS Porting Interface
 I2C.hInter-Integrated Circuit (I2C) Controller Driver
 I2CSupport.hHolder of common helper functions for the I2C driver
 I2CWFF3.hI2C driver implementation for a WiFi F3 device I2C controller
 I2S.hInter-Integrated Circuit Sound (I2S) Bus Driver
 I2SWFF3.hI2S driver implementation for WFF3 devices
 ITM.hITM driver header
 ITMWFF3.hCC35XX specific ITM implementation
 LED.hLED driver
 List.hLinked List interface for use in drivers
 LogSinkBuf.h
 LogSinkITM.hPRELIMINARY LogSinkITM interface
 LogSinkUART.hPRELIMINARY LogSinkUART interface
 Math.hMath utility functions
 MessageQueueP.hMessageQueue module for the RTOS Porting Interface
 MutexP.hMutex module for the RTOS Porting Interface
 NoRTOS.hNoRTOS framework module
 NVS.hNon-Volatile Storage driver interface
 Power.hPower Manager
 PowerWFF3.hPower manager interface for WFF3 devices
 PWM.hPulse Width Modulation (PWM) driver
 PWMTimerWFF3.hPWM driver implementation for Wi-Fi F3 devices
 RingBuf.h
 SD.hSecure Digital (SD) Driver
 SDIO.hSecure Digital Input Output (SDIO) Driver
 SDIOWFF3.h
 SDWFF3.h
 SemaphoreP.hSemaphore module for the RTOS Porting Interface
 SPI.hSerial Peripheral Interface (SPI) Driver Interface
 spiffs.h
 SPIFFSNVS.hModule to enable the SPI Flash File System (SPIFFS) on the TI NVS driver
 SPIWFF3DMA.hSPI driver implementation for a Wi-Fi F3 device SPI controller using the DMA controller
 StructRingBuf.h
 SwiP.hSoftware Interrupt module for the RTOS Porting Interface
 SystemP.hSystem module for the RTOS Porting Interface
 TaskP.hTask module for the RTOS Porting Interface
 TimestampP.hTimestamp module for the RTOS Porting Interface
 types.h
 UART2.hPRELIMINARY UART driver interface
 UART2Support.hHolder of common helper functions for the UART driver
 UART2WFF3.hUART driver implementation for a Low Power F3 device UART controller
 unistd.h
 Watchdog.hWatchdog driver interface
 WatchdogWFF3.hWatchdog driver implementation for WiFi F3 devices
 XMEMWFF3.h
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale