![]() |
![]() |
| C_NoRTOS_Config | NoRTOS framework global configuration |
| CADC_Config_ | ADC driver's custom configuration structure |
| CADC_FxnTable | The definition of an ADC function table that contains the required set of functions to control a specific ADC driver implementation |
| CADC_Params | ADC Parameters used with ADC_open() |
| CADCWFF3_HWAttrs | ADCWFF3 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions |
| CADCWFF3_Object | ADCWFF3 Object |
| CButton_Config | Button configuration |
| CButton_HWAttrs | Hardware specific settings for a button |
| CButton_Object | Internal to Button module. Members should not be accessed by the application |
| CButton_Params | Button Parameters |
| CClockP_FreqHz | Frequency-in-hertz struct |
| CClockP_Params | Basic ClockP Parameters |
| CClockP_Struct | ClockP structure |
| CDisplay_Config | Display Global configuration |
| CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
| CDisplay_Params | Display Parameters |
| CDisplayHost_HWAttrs | DisplayHost Attributes |
| CDisplayHost_Object | DisplayHost Object |
| CDisplayUart2_HWAttrs | DisplayUart2 Attributes |
| CDisplayUart2_Object | DisplayUart2 Object |
| CEventP_Struct | EventP structure |
| CFlashPollingCfg | Flash polling configuration structure |
| CFlashRegister | Flash register structure for address-data pairs |
| CFlashStigEraseCfg | Flash STIG erase configuration structure |
| CFlashStigReadCfg | Flash STIG read configuration structure |
| CFlashStigWriteCfg | Flash STIG write configuration structure |
| CFlashType | Flash type configuration structure |
| CGPIO_Config | GPIO driver configuration structure |
| CGPTimerWFF3_ChannelConf | GPTimerWFF3 channel dependent pin configuration struct |
| CGPTimerWFF3_ChannelProp | GPTimerWFF3 channel dependent properties struct |
| CGPTimerWFF3_Config | GPTimer Global configuration |
| CGPTimerWFF3_HWAttrs | GPTimerWFF3 Hardware attributes |
| CGPTimerWFF3_Object | GPTimerWFF3 Object |
| CGPTimerWFF3_Params | GPTimerWFF3 Parameters |
| CHwiP_Params | Basic HwiP Parameters |
| CHwiP_Struct | HwiP structure |
| CI2C_Config_ | I2C driver's custom configuration structure |
| CI2C_Params | I2C parameters used with I2C_open() |
| CI2C_Transaction | Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout() |
| CI2CWFF3_HWAttrs | I2CWFF3 Hardware attributes |
| CI2CWFF3_Object | I2CWFF3 Object |
| CI2S_Config | I2S Global configuration |
| CI2S_Params | Basic I2S Parameters |
| CI2S_Transaction | I2S transaction descriptor |
| CI2SWFF3_ADFS | Adaptive Digital Frequency Synthesizer (ADFS) |
| CI2SWFF3_HWAttrs | I2S Hardware attributes |
| CITM_HWAttrs | ITM Hardware Attributes |
| CITMWFF3_HWAttrs | |
| CLED_Config | LED configuration |
| CLED_HWAttrs | Hardware specific settings for a LED module |
| CLED_Object | LED Object structure |
| CLED_Params | LED Parameters |
| CList_Elem_ | |
| CList_List | |
| CLogSinkBuf_Instance | |
| CLogSinkBuf_Rec | |
| CLogSinkITM_Instance | |
| CLogSinkUART_Config | LogSinkUART Global configuration |
| CLogSinkUART_HWAttrs | LogSinkUART Hardware attributes |
| CLogSinkUART_Instance | LogSinkUART Sink parameters |
| CLogSinkUART_Object | LogSinkUART Object |
| CMessageQueueP_Struct | MessageQueueP structure |
| CMutexP_Params | Basic MutexP Parameters |
| CMutexP_Struct | MutexP structure |
| CNVS_Attrs | NVS attributes |
| CNVS_Config_ | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CPower_NotifyObj | Power notify object structure |
| CPowerWFF3_Config | Global configuration structure |
| CPWM_Config_ | PWM Global configuration |
| CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params | PWM Parameters |
| CPWMTimerWFF3_HwAttrs | PWMTimerWFF3 Hardware attributes |
| CPWMTimerWFF3_Object | PWMTimerWFF3 Object |
| CRingBuf_Object | |
| CSD_Config_ | SD Global configuration |
| CSD_FxnTable | The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation |
| CSD_Params | SD Parameters |
| CSDIO_Config_ | SDIO Global configuration |
| CSDIO_Params | SDIO Parameters |
| CSDIOWFF3_HwAttrs | |
| CSDIOWFF3_Object | SDIOWFF3 driver object |
| CSDIOWFF3_Param | |
| CSDWFF3_HwAttrs | |
| CSDWFF3_Object | SDWFF3 driver object |
| CSDWFF3_Param | |
| CSemaphoreP_Params | Basic SemaphoreP Parameters |
| CSemaphoreP_Struct | SemaphoreP structure |
| CSPI_Config_ | SPI Global configuration |
| CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params | SPI Parameters |
| CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| Cspiffs_config | |
| Cspiffs_DIR | |
| Cspiffs_dirent | |
| Cspiffs_stat | |
| Cspiffs_t | |
| CSPIFFSNVS_Data_ | SPIFFSNVS data object |
| CSPIFFSNVS_Lock_ | SPIFFSNVS Lock |
| CSPIWFF3DMA_HWAttrs | SPIWFF3DMA Hardware attributes |
| CSPIWFF3DMA_Object | SPIWFF3DMA Object |
| CStructRingBuf_Object | |
| CSwiP_Params | Basic SwiP Parameters |
| CSwiP_Struct | SemaphoreP structure |
| CTaskP_Params | |
| CTaskP_Struct | TaskP structure |
| CTimestampP_Format | |
| CUART2_Config_ | UART2 Global configuration |
| CUART2_Params | UART2 Parameters |
| CUART2WFF3_HWAttrs | UART2WFF3 Hardware attributes |
| CUART2WFF3_Object | UART2WFF3 Object |
| CWatchdog_Config_ | Watchdog Global configuration |
| CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params | Watchdog Parameters |
| CWatchdogWFF3_HWAttrs | Watchdog hardware attributes for WFF3 |
| CWatchdogWFF3_Object | Watchdog Object for WFF3 |
| CXMEM_Attrs | XMEM attributes |
| CXMEM_Config_ | XMEM Global configuration |
| CXMEM_Params | Parameters for opening an XMEM region |
| CXMEMWFF3_HWAttrs | Hardware attributes structure for the XMEMWFF3 driver |
| CXMEMWFF3_Object | Runtime state object for the XMEMWFF3 driver instance |