Data Structures | Typedefs | Enumerations | Functions
SDIOWFF3.h File Reference

Go to the source code of this file.

Data Structures

struct  SDIOWFF3_Object
 SDIOWFF3 driver object. More...
 
struct  SDIOWFF3_HwAttrs
 
struct  SDIOWFF3_Param
 

Typedefs

typedef void(* SDIOWFF3EventCB) (SDIO_Handle handle, uint8_t eventIDX)
 

Enumerations

enum  SDIOWFF_eventIDX {
  SDIOWFF3_DATA_IN_RX_FIFO = 1, SDIOWFF3_CARD_INIT = 2, SDIOWFF3_CARD_DEINIT = 3, SDIOWFF3_RX_CRC_ERROR = 4,
  SDIOWFF3_RX_BUFF_OVERRUN = 5, SDIOWFF3_RX_BUFF_UNDERRUN = 6, SDIOWFF3_TX_BUFF_OVERRUN = 7, SDIOWFF3_TX_BUFF_UNDERRUN = 8,
  SDIOWFF3_HOST_WRONG_ACCESS = 9, SDIOWFF3_HOST_SENT_MSG = 10
}
 

Functions

bool SDIOWFF3_isSdioInitialized (void)
 Function to check if SDIO host already initialize SDIO peripheral SDIO initialize definition is: TRUE - after SDIO host enable SDIO functions FALSE - after SDIO host reset SDIO peripheral. More...
 

Typedef Documentation

§ SDIOWFF3EventCB

typedef void(* SDIOWFF3EventCB) (SDIO_Handle handle, uint8_t eventIDX)

Enumeration Type Documentation

§ SDIOWFF_eventIDX

Enumerator
SDIOWFF3_DATA_IN_RX_FIFO 
SDIOWFF3_CARD_INIT 
SDIOWFF3_CARD_DEINIT 
SDIOWFF3_RX_CRC_ERROR 
SDIOWFF3_RX_BUFF_OVERRUN 
SDIOWFF3_RX_BUFF_UNDERRUN 
SDIOWFF3_TX_BUFF_OVERRUN 
SDIOWFF3_TX_BUFF_UNDERRUN 
SDIOWFF3_HOST_WRONG_ACCESS 
SDIOWFF3_HOST_SENT_MSG 

Function Documentation

§ SDIOWFF3_isSdioInitialized()

bool SDIOWFF3_isSdioInitialized ( void  )

Function to check if SDIO host already initialize SDIO peripheral SDIO initialize definition is: TRUE - after SDIO host enable SDIO functions FALSE - after SDIO host reset SDIO peripheral.

Precondition
SDIO driver has been opened and initialized by calling SDIO_open()
Returns
True if the card is initialized
© Copyright 1995-2026, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale