128 #ifndef ti_drivers_pwm_PWMTimerWFF3__include 129 #define ti_drivers_pwm_PWMTimerWFF3__include GPTimerWFF3_Handle hTimer
Definition: PWMTimerWFF3.h:171
uint32_t periodValue
Definition: PWMTimerWFF3.h:167
PWM_Duty_Units
PWM duty cycle unit definitions. Refer to device specific implementation if using PWM_DUTY_COUNTS (ra...
Definition: PWM.h:306
bool isOpen
Definition: PWMTimerWFF3.h:176
PWMTimerWFF3 Object.
Definition: PWMTimerWFF3.h:165
const PWM_FxnTable PWMTimerWFF3_fxnTable
uint16_t preScalerDivision
Definition: PWMTimerWFF3.h:153
Pulse Width Modulation (PWM) driver.
GPTimer Global configuration.
Definition: GPTimerWFF3.h:809
PWM_Period_Units
PWM period unit definitions. Refer to device specific implementation if using PWM_PERIOD_COUNTS (raw ...
Definition: PWM.h:294
PWM_Period_Units periodUnit
Definition: PWMTimerWFF3.h:172
GPTimerWFF3_ChannelNo
Definitions for supported GPTimer channel numbers.
Definition: GPTimerWFF3.h:283
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:409
struct PWMTimerWFF3_Object PWMTimerWFF3_Object
PWMTimerWFF3 Object.
GPTimerWFF3_ChannelNo chNumber
Definition: PWMTimerWFF3.h:174
GPTimer driver implementation for Wi-Fi F3 devices.
PWM_Duty_Units dutyUnit
Definition: PWMTimerWFF3.h:173
uint32_t dutyCounts
Definition: PWMTimerWFF3.h:170
PWMTimerWFF3 Hardware attributes.
Definition: PWMTimerWFF3.h:150
uint8_t gpTimerInstance
Definition: PWMTimerWFF3.h:152
uint32_t dutyValue
Definition: PWMTimerWFF3.h:169
struct PWMTimerWFF3_HwAttrs PWMTimerWFF3_HwAttrs
PWMTimerWFF3 Hardware attributes.
PWM_IdleLevel
Idle output level when PWM is not running (stopped / not started).
Definition: PWM.h:321
bool isRunning
Definition: PWMTimerWFF3.h:177
uint32_t periodCounts
Definition: PWMTimerWFF3.h:168
PWM_IdleLevel idleLevel
Definition: PWMTimerWFF3.h:175