CC35xxDriverLibrary

#include <ospi.h>

Data Fields

uint8_t stigOpcode
 
uint8_t stigRdEn
 
uint8_t stigRDNumBytes
 
uint8_t stigAddrEn
 
uint8_t stigAddrNumBytes
 
uint8_t stigModeBitEN
 
uint8_t stigWrEn
 
uint8_t stigWrNumBytes
 
uint8_t stigNumDummyCycles
 
uint8_t stigMemoryEn
 

Field Documentation

§ stigOpcode

uint8_t OSPISTIGConfig_t::stigOpcode

Referenced by OSPISetSTIGDataRegister().

§ stigRdEn

uint8_t OSPISTIGConfig_t::stigRdEn

Referenced by OSPISetSTIGDataRegister().

§ stigRDNumBytes

uint8_t OSPISTIGConfig_t::stigRDNumBytes

Referenced by OSPISetSTIGDataRegister().

§ stigAddrEn

uint8_t OSPISTIGConfig_t::stigAddrEn

Referenced by OSPISetSTIGDataRegister().

§ stigAddrNumBytes

uint8_t OSPISTIGConfig_t::stigAddrNumBytes

Referenced by OSPISetSTIGDataRegister().

§ stigModeBitEN

uint8_t OSPISTIGConfig_t::stigModeBitEN

Referenced by OSPISetSTIGDataRegister().

§ stigWrEn

uint8_t OSPISTIGConfig_t::stigWrEn

Referenced by OSPISetSTIGDataRegister().

§ stigWrNumBytes

uint8_t OSPISTIGConfig_t::stigWrNumBytes

Referenced by OSPISetSTIGDataRegister().

§ stigNumDummyCycles

uint8_t OSPISTIGConfig_t::stigNumDummyCycles

Referenced by OSPISetSTIGDataRegister().

§ stigMemoryEn

uint8_t OSPISTIGConfig_t::stigMemoryEn

The documentation for this struct was generated from the following file: