25 #ifndef __CMSIS_COMPILER_H 26 #define __CMSIS_COMPILER_H 33 #if defined ( __CC_ARM ) 34 #include "cmsis_armcc.h" 40 #elif defined (__ARMCC_VERSION) && (__ARMCC_VERSION >= 6010050) && (__ARMCC_VERSION < 6100100) 41 #include "cmsis_armclang_ltm.h" 46 #elif defined (__ARMCC_VERSION) && (__ARMCC_VERSION >= 6100100) 47 #include "cmsis_armclang.h" 53 #elif defined ( __GNUC__ ) || defined(__clang__) 60 #elif defined ( __ICCARM__ ) 67 #elif defined ( __TI_ARM__ ) 68 #include "cmsis_ccs.h" 74 #define __INLINE inline 76 #ifndef __STATIC_INLINE 77 #define __STATIC_INLINE static inline 79 #ifndef __STATIC_FORCEINLINE 80 #define __STATIC_FORCEINLINE __STATIC_INLINE 83 #define __NO_RETURN __attribute__((noreturn)) 86 #define __USED __attribute__((used)) 89 #define __WEAK __attribute__((weak)) 92 #define __PACKED __attribute__((packed)) 94 #ifndef __PACKED_STRUCT 95 #define __PACKED_STRUCT struct __attribute__((packed)) 97 #ifndef __PACKED_UNION 98 #define __PACKED_UNION union __attribute__((packed)) 100 #ifndef __UNALIGNED_UINT32 102 #define __UNALIGNED_UINT32(x) (((struct T_UINT32 *)(x))->v) 104 #ifndef __UNALIGNED_UINT16_WRITE 106 #define __UNALIGNED_UINT16_WRITE(addr, val) (void)((((struct T_UINT16_WRITE *)(void*)(addr))->v) = (val)) 108 #ifndef __UNALIGNED_UINT16_READ 110 #define __UNALIGNED_UINT16_READ(addr) (((const struct T_UINT16_READ *)(const void *)(addr))->v) 112 #ifndef __UNALIGNED_UINT32_WRITE 114 #define __UNALIGNED_UINT32_WRITE(addr, val) (void)((((struct T_UINT32_WRITE *)(void *)(addr))->v) = (val)) 116 #ifndef __UNALIGNED_UINT32_READ 118 #define __UNALIGNED_UINT32_READ(addr) (((const struct T_UINT32_READ *)(const void *)(addr))->v) 121 #define __ALIGNED(x) __attribute__((aligned(x))) 124 #define __RESTRICT __restrict 126 #ifndef __COMPILER_BARRIER 127 #warning No compiler specific solution for __COMPILER_BARRIER. __COMPILER_BARRIER is ignored. 128 #define __COMPILER_BARRIER() (void)0 135 #elif defined ( __TASKING__ ) 146 #define __INLINE inline 148 #ifndef __STATIC_INLINE 149 #define __STATIC_INLINE static inline 151 #ifndef __STATIC_FORCEINLINE 152 #define __STATIC_FORCEINLINE __STATIC_INLINE 155 #define __NO_RETURN __attribute__((noreturn)) 158 #define __USED __attribute__((used)) 161 #define __WEAK __attribute__((weak)) 164 #define __PACKED __packed__ 166 #ifndef __PACKED_STRUCT 167 #define __PACKED_STRUCT struct __packed__ 169 #ifndef __PACKED_UNION 170 #define __PACKED_UNION union __packed__ 172 #ifndef __UNALIGNED_UINT32 173 struct __packed__ T_UINT32 { uint32_t v; };
174 #define __UNALIGNED_UINT32(x) (((struct T_UINT32 *)(x))->v) 176 #ifndef __UNALIGNED_UINT16_WRITE 178 #define __UNALIGNED_UINT16_WRITE(addr, val) (void)((((struct T_UINT16_WRITE *)(void *)(addr))->v) = (val)) 180 #ifndef __UNALIGNED_UINT16_READ 182 #define __UNALIGNED_UINT16_READ(addr) (((const struct T_UINT16_READ *)(const void *)(addr))->v) 184 #ifndef __UNALIGNED_UINT32_WRITE 186 #define __UNALIGNED_UINT32_WRITE(addr, val) (void)((((struct T_UINT32_WRITE *)(void *)(addr))->v) = (val)) 188 #ifndef __UNALIGNED_UINT32_READ 190 #define __UNALIGNED_UINT32_READ(addr) (((const struct T_UINT32_READ *)(const void *)(addr))->v) 193 #define __ALIGNED(x) __align(x) 196 #warning No compiler specific solution for __RESTRICT. __RESTRICT is ignored. 199 #ifndef __COMPILER_BARRIER 200 #warning No compiler specific solution for __COMPILER_BARRIER. __COMPILER_BARRIER is ignored. 201 #define __COMPILER_BARRIER() (void)0 208 #elif defined ( __CSMC__ ) 209 #include <cmsis_csm.h> 215 #define __INLINE inline 217 #ifndef __STATIC_INLINE 218 #define __STATIC_INLINE static inline 220 #ifndef __STATIC_FORCEINLINE 221 #define __STATIC_FORCEINLINE __STATIC_INLINE 228 #warning No compiler specific solution for __USED. __USED is ignored. 232 #define __WEAK __weak 235 #define __PACKED @packed 237 #ifndef __PACKED_STRUCT 238 #define __PACKED_STRUCT @packed struct 240 #ifndef __PACKED_UNION 241 #define __PACKED_UNION @packed union 243 #ifndef __UNALIGNED_UINT32 244 @packed
struct T_UINT32 { uint32_t v; };
245 #define __UNALIGNED_UINT32(x) (((struct T_UINT32 *)(x))->v) 247 #ifndef __UNALIGNED_UINT16_WRITE 249 #define __UNALIGNED_UINT16_WRITE(addr, val) (void)((((struct T_UINT16_WRITE *)(void *)(addr))->v) = (val)) 251 #ifndef __UNALIGNED_UINT16_READ 253 #define __UNALIGNED_UINT16_READ(addr) (((const struct T_UINT16_READ *)(const void *)(addr))->v) 255 #ifndef __UNALIGNED_UINT32_WRITE 257 #define __UNALIGNED_UINT32_WRITE(addr, val) (void)((((struct T_UINT32_WRITE *)(void *)(addr))->v) = (val)) 259 #ifndef __UNALIGNED_UINT32_READ 261 #define __UNALIGNED_UINT32_READ(addr) (((const struct T_UINT32_READ *)(const void *)(addr))->v) 264 #warning No compiler specific solution for __ALIGNED. __ALIGNED is ignored. 268 #warning No compiler specific solution for __RESTRICT. __RESTRICT is ignored. 271 #ifndef __COMPILER_BARRIER 272 #warning No compiler specific solution for __COMPILER_BARRIER. __COMPILER_BARRIER is ignored. 273 #define __COMPILER_BARRIER() (void)0 278 #error Unknown compiler. CMSIS compiler GCC header file.
uint32_t __attribute__((section(".TI.ramfunc")))
Definition: ospi.c:52
__PACKED_STRUCT T_UINT16_WRITE
Definition: cmsis_gcc.h:82
#define __PACKED_STRUCT
Definition: cmsis_gcc.h:65
__PACKED_STRUCT T_UINT32_WRITE
Definition: cmsis_gcc.h:98
CMSIS compiler ICCARM (IAR Compiler for Arm) header file.
__PACKED_STRUCT T_UINT32_READ
Definition: cmsis_gcc.h:106
__PACKED_STRUCT T_UINT16_READ
Definition: cmsis_gcc.h:90