CC35xxDriverLibrary
MISRA-C:2004 Compliance Exceptions

CMSIS violates the following MISRA-C:2004 rules:

  • Required Rule 8.5, object/function definition in header file.
    Function definitions in header files are used to allow 'inlining'.
  • Required Rule 18.4, declaration of union type or object of union type: '{...}'.
    Unions are used for effective representation of core registers.
  • Advisory Rule 19.7, Function-like macro defined.
    Function-like macros are used to allow more efficient code.