AM261x MCU+ SDK  26.00.00
sdl_soc_rti.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2024
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  *
32  */
33 
34 #ifndef SDL_SOC_RTI_H_
35 #define SDL_SOC_RTI_H_
36 
37 #include <sdl/include/am261x/sdlr_soc_baseaddress.h>
38 
39 #ifdef __cplusplus
40 extern "C" {
41 #endif
42 
43 /*
44 * Required Macros for Instances config
45 */
46 
47 #define SDL_RTI_MAX_INSTANCE (0x02U)
48 #define INSTANCE_INVALID (0x0U)
49 
60 /*************************************************************************************************************
61 * Enum for different RTI module instances
62 **************************************************************************************************************/
63 
64 typedef enum {
65 
69 
71 
72 
75 /*======================================================================================================
76 * This is global array gives the BASE ADDRESS of RTI modules
77 ======================================================================================================*/
78 
79 static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U] = {SDL_WDT0_U_BASE,SDL_WDT1_U_BASE,
81 
83  uint32_t *baseAddr);
84 
85 #ifdef __cplusplus
86 }
87 #endif
88 
89 #endif /* SDL_SOC_RTI_H_ */
SDL_INSTANCE_WDT0
@ SDL_INSTANCE_WDT0
Definition: sdl_soc_rti.h:66
INSTANCE_INVALID
#define INSTANCE_INVALID
Definition: sdl_soc_rti.h:48
SDL_INSTANCE_INVALID
@ SDL_INSTANCE_INVALID
Definition: sdl_soc_rti.h:68
SDL_INSTANCE_WDT1
@ SDL_INSTANCE_WDT1
Definition: sdl_soc_rti.h:67
SDL_RTI_MAX_INSTANCE
#define SDL_RTI_MAX_INSTANCE
Definition: sdl_soc_rti.h:47
SDL_RTI_baseAddress
static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U]
Definition: sdl_soc_rti.h:79
SDL_RTI_InstanceType
SDL_RTI_InstanceType
Definition: sdl_soc_rti.h:64
SDL_RTI_getBaseaddr
int32_t SDL_RTI_getBaseaddr(SDL_RTI_InstanceType instance, uint32_t *baseAddr)