AM261x MCU+ SDK  26.00.00
sdl_ecc_core.h
Go to the documentation of this file.
1 /*
2  * SDL ECC
3  *
4  * Software Diagnostics Library module for ECC
5  *
6  * Copyright (c) Texas Instruments Incorporated 2023
7  *
8  * Redistribution and use in source and binary forms, with or without
9  * modification, are permitted provided that the following conditions
10  * are met:
11  *
12  * Redistributions of source code must retain the above copyright
13  * notice, this list of conditions and the following disclaimer.
14  *
15  * Redistributions in binary form must reproduce the above copyright
16  * notice, this list of conditions and the following disclaimer in the
17  * documentation and/or other materials provided with the
18  * distribution.
19  *
20  * Neither the name of Texas Instruments Incorporated nor the names of
21  * its contributors may be used to endorse or promote products derived
22  * from this software without specific prior written permission.
23  *
24  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
25  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
26  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
27  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
28  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
29  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
30  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
31  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
32  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
33  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
34  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
35  *
36  */
37 
38 #ifndef INCLUDE_SDL_ECC_CORE_H_
39 #define INCLUDE_SDL_ECC_CORE_H_
40 
41 #include <stdint.h>
42 #include <sdl/sdl_ecc.h>
43 
44 int32_t SDL_ECC_configECCRam(uint32_t ramId);
45 
47  SDL_ECC_MemSubType memSubType,
48  SDL_ECC_InjectErrorType errorType);
49 #endif /* INCLUDE_SDL_ECC_CORE_H_ */
SDL_ECC_InjectErrorType
SDL_ECC_InjectErrorType
ECC Inject error types.
Definition: sdl_ecc.h:303
sdl_ecc.h
Header file contains enumerations, structure definitions and function.
SDL_ECC_pollErrorEvent
uint32_t SDL_ECC_pollErrorEvent(SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType)
SDL_ECC_MemSubType
uint32_t SDL_ECC_MemSubType
This enumerator indicate ECC memory Sub Type.
Definition: sdl_ecc.h:341
SDL_ECC_configECCRam
int32_t SDL_ECC_configECCRam(uint32_t ramId)
SDL_ECC_MemType
uint32_t SDL_ECC_MemType
This enumerator indicate ECC memory type.
Definition: sdl_ecc.h:348