AM261x MCU+ SDK  26.00.00
VTM IP Functions

Introduction

Functions

SDL_VTM_adc_code SDL_VTM_getAdcCode (SDL_VTM_InstTs instance)
 read Temperature sensor ADC code More...
 
int32_t SDL_VTM_tsGetCtrl (SDL_VTM_InstTs instance, uint32_t *pTsCtrlCfg)
 Read VTM Temperature Sensor Control. More...
 
int32_t SDL_VTM_tsConvADCToTemp (SDL_VTM_adc_code adcCode, int32_t *pMilliDegreeTempVal)
 VTM Temperature ADC code to Temperature conversion. More...
 
int32_t SDL_VTM_tsConvTempToAdc (int32_t milliDegreeTempVal, SDL_VTM_adc_code *pAdcCode)
 VTM Temperature to ADC code conversion. More...
 

Function Documentation

◆ SDL_VTM_getAdcCode()

SDL_VTM_adc_code SDL_VTM_getAdcCode ( SDL_VTM_InstTs  instance)

read Temperature sensor ADC code

Parameters
instance[IN] sensor for which ADC code is needed
Returns
The SDL SDL_VTM_adc_code

◆ SDL_VTM_tsGetCtrl()

int32_t SDL_VTM_tsGetCtrl ( SDL_VTM_InstTs  instance,
uint32_t *  pTsCtrlCfg 
)

Read VTM Temperature Sensor Control.

Parameters
instance[IN] VTM Temperature sensor instance
pTsCtrlCfg[IN] Pointer to temperature sensor control configuration
Returns
The SDL error code for the API. Success : SDL_PASS Fail : SDL_EFAIL Invalid Args : SDL_EBADARGS

◆ SDL_VTM_tsConvADCToTemp()

int32_t SDL_VTM_tsConvADCToTemp ( SDL_VTM_adc_code  adcCode,
int32_t *  pMilliDegreeTempVal 
)

VTM Temperature ADC code to Temperature conversion.

Parameters
adcCode[IN] 7 Bit ADC code
pMilliDegreeTempVal[OUT] Pointer to Temperature in milli degree celcius
Returns
The SDL error code for the API. Success : SDL_PASS Invalid Args : SDL_EBADARGS

◆ SDL_VTM_tsConvTempToAdc()

int32_t SDL_VTM_tsConvTempToAdc ( int32_t  milliDegreeTempVal,
SDL_VTM_adc_code pAdcCode 
)

VTM Temperature to ADC code conversion.

Parameters
milliDegreeTempVal[IN] Temperature in milli degree celcius
pAdcCode[OUT] Pointer to 7 Bit ADC code
Returns
The SDL error code for the API. Success : SDL_PASS Invalid Args : SDL_EBADARGS