AM261x MCU+ SDK  26.00.00
Generic NOR Flash API for single pin mode

Introduction

These APIs try to communicate with whichever flash is connected the OSPI peripheral in 1-1-1 mode. This can be used in bringing up new flashes and mostly used for debug and diagnostic purposes

Functions

int32_t OSPI_lld_norFlashInit1s1s1s (OSPILLD_Handle handle)
 This function initializes the NOR flash to work in 1-1-1 mode. More...
 
void OSPI_lld_norFlashSetCmds (uint8_t rdCmd, uint8_t wrCmd, uint8_t eraseCmd)
 This function sets up internal bookkeeping variables for read, write and erase commands. This API has to be called immediately before OSPI_lld_norFlashInit1s1s1s. More...
 
int32_t OSPI_lld_norFlashReadId (OSPILLD_Handle handle, uint32_t *manufacturerId, uint32_t *deviceId)
 This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral. More...
 
int32_t OSPI_lld_norFlashWrite (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function writes data to the flash at a specified offset. More...
 
int32_t OSPI_lld_norFlashRead (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads data from the flash from a specified offset in DAC mode. More...
 
int32_t OSPI_lld_norFlashReadIndirect (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads data from the flash from a specified offset in INDAC mode. More...
 
int32_t OSPI_lld_norFlashReadSfdp (OSPILLD_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
 This function reads SFDP table from the flash from a specified offset. More...
 
int32_t OSPI_lld_norFlashErase (OSPILLD_Handle handle, uint32_t address)
 This function erases 1 block of data starting from a provided address. More...
 
int32_t OSPI_lld_configResetPin (OSPILLD_Handle handle, uint32_t config)
 This function configures reset functionality. More...
 
int32_t OSPI_lld_configBaudrate (OSPILLD_Handle handle, uint32_t baud)
 Configures baud divider. More...
 
int32_t OSPI_lld_readBaudRateDivFromReg (OSPILLD_Handle handle, uint32_t *baudDiv)
 Return value of baudrate that is programmed in IP register. More...
 
int32_t OSPI_lld_getBaudRateDivFromObj (OSPILLD_Handle handle, uint32_t *baudDiv)
 Return value of baudrate that is saved in OSPI Object. More...
 
int32_t OSPI_lld_setResetPinStatus (OSPILLD_Handle hOspi, uint32_t pinStatus)
 This function activates the RESET pin feature. More...
 
int32_t OSPI_dmaOpen (OSPILLD_Handle hOspi)
 API to open an OSPI DMA channel. More...
 
int32_t OSPI_dmaClose (OSPILLD_Handle handle)
 API to close an OSPI DMA channel. More...
 
int32_t OSPI_dmaCopy (OSPILLD_Handle handle, void *dst, void *src, uint32_t length, uint32_t timeout)
 API to do a DMA Copy using appropriate DMA Channel opened. More...
 
int32_t OSPI_isDmaInterruptEnabled (OSPILLD_Handle handle)
 API to get the DMA Interrupt status. More...
 
int32_t OSPI_lld_phyValidateTuningPoint (OSPILLD_Handle hOspi, uint32_t flashOffset)
 Validates a tuning point for the OSPI physical interface. More...
 
uint32_t OSPI_lld_isValidateOtpEnable (OSPILLD_Handle hOspi)
 Checks if OTP validation is enabled for the OSPI controller. More...
 
int32_t OSPI_lld_setFrequency (OSPILLD_Handle hOspi, uint64_t inputClkFreq)
 Sets the operating frequency for the OSPI peripheral. More...
 
int32_t OSPI_lld_setDelays (OSPILLD_Handle hOspi, uint32_t inputClkFreq)
 Sets timing delays for the OSPI interface based on input clock frequency. More...
 
int32_t OSPI_lld_setBaudRateDiv (OSPILLD_Handle hOspi, uint32_t baudRateDiv)
 Sets the baud rate divider for OSPI communication. More...
 
int32_t OSPI_lld_disableDdrRdCmds (OSPILLD_Handle hOspi)
 This function resets DDR bit in INSTR_RD register for RD commands. More...
 
int32_t OSPI_lld_set1sProtocol (OSPILLD_Handle hOspi)
 Resets the OSPI controller to operate in 1S-1S-1S mode. More...
 

Function Documentation

◆ OSPI_lld_norFlashInit1s1s1s()

int32_t OSPI_lld_norFlashInit1s1s1s ( OSPILLD_Handle  handle)

This function initializes the NOR flash to work in 1-1-1 mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashSetCmds()

void OSPI_lld_norFlashSetCmds ( uint8_t  rdCmd,
uint8_t  wrCmd,
uint8_t  eraseCmd 
)

This function sets up internal bookkeeping variables for read, write and erase commands. This API has to be called immediately before OSPI_lld_norFlashInit1s1s1s.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
rdCmdCommand to be used in single mode read
wrCmdCommand to be used in single mode write/page program
eraseCmdCommand to be used to erase (block or sector)

◆ OSPI_lld_norFlashReadId()

int32_t OSPI_lld_norFlashReadId ( OSPILLD_Handle  handle,
uint32_t *  manufacturerId,
uint32_t *  deviceId 
)

This function tries to read the JEDEC ID from the NOR flash connected to the OSPI peripheral.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
manufacturerIdPointer to a uint32_t variable. This will be filled with the manufacturer ID on success
deviceIdPointer to a uint32_t variable. This will be filled with the device ID on success
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashWrite()

int32_t OSPI_lld_norFlashWrite ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function writes data to the flash at a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be written
bufBuffer which has the data to be written to the flash
lenNumber of bytes to be written to the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashRead()

int32_t OSPI_lld_norFlashRead ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads data from the flash from a specified offset in DAC mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashReadIndirect()

int32_t OSPI_lld_norFlashReadIndirect ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads data from the flash from a specified offset in INDAC mode.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashReadSfdp()

int32_t OSPI_lld_norFlashReadSfdp ( OSPILLD_Handle  handle,
uint32_t  offset,
uint8_t *  buf,
uint32_t  len 
)

This function reads SFDP table from the flash from a specified offset.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
offsetOffset at which the data is to be read from
bufBuffer to which data will be written into
lenNumber of bytes to be read from the flash
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_norFlashErase()

int32_t OSPI_lld_norFlashErase ( OSPILLD_Handle  handle,
uint32_t  address 
)

This function erases 1 block of data starting from a provided address.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_open()
addressAddress of the data block to be erased. This address should be block aligned.
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_configResetPin()

int32_t OSPI_lld_configResetPin ( OSPILLD_Handle  handle,
uint32_t  config 
)

This function configures reset functionality.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
configreset config
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_configBaudrate()

int32_t OSPI_lld_configBaudrate ( OSPILLD_Handle  handle,
uint32_t  baud 
)

Configures baud divider.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
baudbaudrate from 2 to 32 and divisible by 2
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_readBaudRateDivFromReg()

int32_t OSPI_lld_readBaudRateDivFromReg ( OSPILLD_Handle  handle,
uint32_t *  baudDiv 
)

Return value of baudrate that is programmed in IP register.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPI_Handle returned from an OSPI_open()
baudDivpointer to memory into which baudrate will be written
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_getBaudRateDivFromObj()

int32_t OSPI_lld_getBaudRateDivFromObj ( OSPILLD_Handle  handle,
uint32_t *  baudDiv 
)

Return value of baudrate that is saved in OSPI Object.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
handleAn OSPILLD_Handle returned from an OSPI_init()
baudDivpointer to memory into which baudrate will be written
Returns
OSPI_SYSTEM_SUCCESS on success, OSPI_SYSTEM_FAILURE otherwise

◆ OSPI_lld_setResetPinStatus()

int32_t OSPI_lld_setResetPinStatus ( OSPILLD_Handle  hOspi,
uint32_t  pinStatus 
)

This function activates the RESET pin feature.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
hOspiAn OSPILLD_Handle returned from an OSPI_open()
pinStatuspinStatus - HIGH/LOW
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_dmaOpen()

int32_t OSPI_dmaOpen ( OSPILLD_Handle  hOspi)

API to open an OSPI DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks and the registered via Sysconfig

Parameters
hOspiAn OSPILLD_Handle returned from an OSPI_open()
Returns
SystemP_SUCCESS on success, else failure

◆ OSPI_dmaClose()

int32_t OSPI_dmaClose ( OSPILLD_Handle  handle)

API to close an OSPI DMA channel.

This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig

Parameters
handle[in] An OSPILLD_Handle returned from an OSPI_open()
Returns
SystemP_SUCCESS on success, else failure

◆ OSPI_dmaCopy()

int32_t OSPI_dmaCopy ( OSPILLD_Handle  handle,
void *  dst,
void *  src,
uint32_t  length,
uint32_t  timeout 
)

API to do a DMA Copy using appropriate DMA Channel opened.

This API will open a DMA Channel using the appropriate DMA driver callbacks registered via Sysconfig

Parameters
handle[in] An OSPILLD_Handle returned from an OSPI_open()
dst[in] Destination address to which the data is to be copied
src[in] Source address from which the data is to be copied
length[in] Data length
timeout[in] Timeout for the transaction
Returns
SystemP_SUCCESS on success, else failure

◆ OSPI_isDmaInterruptEnabled()

int32_t OSPI_isDmaInterruptEnabled ( OSPILLD_Handle  handle)

API to get the DMA Interrupt status.

This API will retrieve the interrrupt status of the DMA Channel

Parameters
handle[in] An OSPILLD_Handle returned from an OSPI_open()
Returns
SystemP_SUCCESS on success, else failure

◆ OSPI_lld_phyValidateTuningPoint()

int32_t OSPI_lld_phyValidateTuningPoint ( OSPILLD_Handle  hOspi,
uint32_t  flashOffset 
)

Validates a tuning point for the OSPI physical interface.

This function verifies if the current OSPI physical interface configuration (tuning point) is valid by performing a read operation at the specified flash offset.

Parameters
hOspiOSPI LLD handle
flashOffsetFlash memory offset to use for the validation read operation
Returns
SystemP_SUCCESS on success, SystemP_FAILURE otherwise

◆ OSPI_lld_isValidateOtpEnable()

uint32_t OSPI_lld_isValidateOtpEnable ( OSPILLD_Handle  hOspi)

Checks if OTP validation is enabled for the OSPI controller.

This function determines whether the OTP (One-Time Programmable) validation feature is currently enabled in the OSPI controller.

Parameters
hOspiHandle to the OSPI controller instance
Returns
uint32_t Returns 1 if OTP validation is enabled, 0 otherwise

◆ OSPI_lld_setFrequency()

int32_t OSPI_lld_setFrequency ( OSPILLD_Handle  hOspi,
uint64_t  inputClkFreq 
)

Sets the operating frequency for the OSPI peripheral.

This function configures the OSPI controller to operate at the specified frequency based on the input clock frequency provided.

Parameters
hOspiOSPI LLD handle
inputClkFreqInput clock frequency in Hz
Returns
SystemP_SUCCESS on success, error code on failure

◆ OSPI_lld_setDelays()

int32_t OSPI_lld_setDelays ( OSPILLD_Handle  hOspi,
uint32_t  inputClkFreq 
)

Sets timing delays for the OSPI interface based on input clock frequency.

This function configures the appropriate timing delays for the OSPI interface to ensure reliable communication with external memory devices. The delays are calculated based on the provided input clock frequency.

Parameters
hOspiOSPI LLD handle
inputClkFreqInput clock frequency in Hz
Returns
SystemP_SUCCESS on success, error code on failure

◆ OSPI_lld_setBaudRateDiv()

int32_t OSPI_lld_setBaudRateDiv ( OSPILLD_Handle  hOspi,
uint32_t  baudRateDiv 
)

Sets the baud rate divider for OSPI communication.

This function configures the baud rate divider to control the OSPI clock frequency. The actual OSPI clock frequency is determined by dividing the input clock frequency by the specified baud rate divider.

Parameters
hOspiOSPI LLD handle
baudRateDivBaud rate divider value
Returns
SystemP_SUCCESS on success, error code on failure

◆ OSPI_lld_disableDdrRdCmds()

int32_t OSPI_lld_disableDdrRdCmds ( OSPILLD_Handle  hOspi)

This function resets DDR bit in INSTR_RD register for RD commands.

Precondition
OSPI controller has been opened using OSPI_open()
Parameters
hOspiAn OSPILLD_Handle returned from an OSPI_open()
Returns
OSPI_SYSTEM_SUCCESS if DDR successfully disabled, else error on failure

◆ OSPI_lld_set1sProtocol()

int32_t OSPI_lld_set1sProtocol ( OSPILLD_Handle  hOspi)

Resets the OSPI controller to operate in 1S-1S-1S mode.

This function reverts the OSPI controller configuration from advanced modes (such as 8D-8D-8D DDR mode) back to the basic single-lane mode (1S-1S-1S). It unsets all registers that were configured for high-performance modes, allowing the controller to operate in the standard SPI mode.

Parameters
hOspiAn OSPILLD_Handle returned from an OSPI_open()
Returns
SystemP_SUCCESS on success, else failure