AM261x MCU+ SDK  26.00.00

Introduction

This module contains APIs to program the MPU Firewall module.

Files

file  mpu_firewall/v0/mpu_firewall.h
 MPU Firewall Driver API/interface file.
 

Data Structures

struct  Firewall_Target
 MPU Firewall Target. More...
 
struct  MPU_FIREWALL_Config
 MPU Firewall Parameters. More...
 
struct  MPU_FIREWALL_RegionParams
 MPU Region Parameters. More...
 

Functions

Fwl_Return_t MPU_FIREWALL_getRegion (MPU_FIREWALL_RegionParams *mpuParams)
 Retrieves the start and end addresses and the permission attributes of a given region in a given firewall. More...
 
Fwl_Return_t MPU_FIREWALL_getFirewallConfig (uint32_t firewallId, MPU_FIREWALL_Config **firewallConfig)
 Function to get parameters associated to a MPU firewall. More...
 
Fwl_Return_t MPU_FIREWALL_readFaultAddress (uint32_t firewallId, uint32_t *faultAddress)
 Function to read the fault address that created the firewall violation. More...
 
Fwl_Return_t MPU_FIREWALL_readFaultStatus (uint32_t firewallId, uint32_t *faultStatus)
 Function to read the fault status register. It contains information on the kind of firewall violation that had occurred. More...
 
Fwl_Return_t MPU_FIREWALL_getInterruptStatus (uint32_t firewallId, uint32_t *interruptStatus)
 Function to read interrupt status. More...
 

Enumerations

enum  Fwl_Return_t { FWL_DRV_RETURN_SUCCESS = 0xBA14D51BU, FWL_DRV_RETURN_FAILURE = 0xAADF4AFAU }
 Firewall Driver Error code. More...
 

Enumeration Type Documentation

◆ Fwl_Return_t

Firewall Driver Error code.

The enumeration describes all the possible return and error codes which the Firewall Driver can return

Enumerator
FWL_DRV_RETURN_SUCCESS 

Success/pass return code

FWL_DRV_RETURN_FAILURE 

General or unspecified failure/error

Function Documentation

◆ MPU_FIREWALL_getRegion()

Fwl_Return_t MPU_FIREWALL_getRegion ( MPU_FIREWALL_RegionParams mpuParams)

Retrieves the start and end addresses and the permission attributes of a given region in a given firewall.

Parameters
mpuParamsStructure containing all region configuration parameters.
Returns
FWL_DRV_RETURN_SUCCESS if the region configuration is successfully fetched; else FWL_DRV_RETURN_FAILURE

◆ MPU_FIREWALL_getFirewallConfig()

Fwl_Return_t MPU_FIREWALL_getFirewallConfig ( uint32_t  firewallId,
MPU_FIREWALL_Config **  firewallConfig 
)

Function to get parameters associated to a MPU firewall.

Parameters
firewallIdFirewall ID.
firewallConfigStructure to save mpu firewall configuration.
Returns
FWL_DRV_RETURN_SUCCESS on successful config read; else FWL_DRV_RETURN_FAILURE

◆ MPU_FIREWALL_readFaultAddress()

Fwl_Return_t MPU_FIREWALL_readFaultAddress ( uint32_t  firewallId,
uint32_t *  faultAddress 
)

Function to read the fault address that created the firewall violation.

Parameters
firewallIdMPU Firewall Id
faultAddresspointer to the faultAddress to be populated
Returns
FWL_DRV_RETURN_SUCCESS on successful fault address read; else FWL_DRV_RETURN_FAILURE

◆ MPU_FIREWALL_readFaultStatus()

Fwl_Return_t MPU_FIREWALL_readFaultStatus ( uint32_t  firewallId,
uint32_t *  faultStatus 
)

Function to read the fault status register. It contains information on the kind of firewall violation that had occurred.

Parameters
firewallIdMPU Firewall Id
faultStatuspointer to the faultStatus to be populated
Returns
FWL_DRV_RETURN_SUCCESS on successful fault status read; else FWL_DRV_RETURN_FAILURE

◆ MPU_FIREWALL_getInterruptStatus()

Fwl_Return_t MPU_FIREWALL_getInterruptStatus ( uint32_t  firewallId,
uint32_t *  interruptStatus 
)

Function to read interrupt status.

Parameters
firewallIdMPU Firewall Id
interruptStatuspointer to the interruptStatus to be populated
Returns
FWL_DRV_RETURN_SUCCESS on successful interrupt status read; else FWL_DRV_RETURN_FAILURE