AM261x MCU+ SDK  26.00.00
SDL R5F ECC ATCM0

Introduction

This example demonstrates the usage of the SDL R5F ATCM0 module. The example shows how to setup and use the ECC Safety Diagnostic operation. Shows the generation of SEC and DED error on R5F ATCM0 ECC Aggregator.

Use Cases

Supported Combinations

Steps to Run the Example

See Also

ECC : Error Correcting Code

Sample Output

Shown below is a sample output when the application is run,