AM261x MCU+ SDK  26.00.00
SDL ECC MSS TPTC

Introduction

This example demonstrates SEC and DED on MSS TPTC FIFO memories.

Use Cases

Use Case Description
UC-1 Single bit error injection.
UC-2 Double bit error injection.

Supported Combinations

Steps to Run the Example

See Also

ECC : Error Correcting Code

Sample Output

Shown below is a sample output when the application is run,