AM261x MCU+ SDK  26.00.00
Optiflash XIP Benchmark with 8KB L2 Cache

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am261x-lp, am261x-som
Example folder examples/benchmarks/optiflash_benchmark/flash_xip_l2_cache_8k

Introduction

This is the same application as Optiflash OCRAM Benchmark, however, target functions are kept in external flash and L2 cache of 8KB is enabled. The effect of it is seen in the execution time.

Steps to Run the Example

Building the application

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Running the application

Flash the application binary to the device, follow the steps mentioned here (see Flash a Hello World example).

Sample output

Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 6 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init : 497us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 96us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 1us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 4478us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 3609us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 8us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 8692us
Image loading done, switching to application ...
OCMC benchmarking:: Board_init success
Filling up the buffers
master_task
master_task -- start sending
memcpy Exec Time I$ Miss I$ Acc INST ICM/sec INST/sec
0B 34698us 86508 1075578 2170054 3.1 77.2
100B 35409us 86897 1223210 2359503 3.0 82.3
200B 35433us 85547 1373892 2559390 3.0 89.2
400B 36996us 86875 1675846 2961500 2.9 98.9
700B 37410us 83367 2116356 3547053 2.8 117.1
1000B 40295us 86212 2579598 4161845 2.6 127.6
1500B 43573us 84025 3326077 5154199 2.4 146.1
2250B 50173us 86438 4470091 6668695 2.1 164.1
2500B 52256us 86831 4834398 7156358 2.1 169.1
4096B 63264us 86107 7233876 10351522 1.7 202.1
All tests have passed