AM261x MCU+ SDK  26.00.00
FreeRTOS MPU Task Switch Example

Introduction

This example shows usage of direct FreeRTOS APIs, i.e not via the DPL APIs. It shows usage of user mode task create API, task notification APIs, semaphore APIs. It also shows how to signal to FreeRTOS task from ISRs.

The example does below:-

  • Creates two user mode tasks, ping and pong with task specific MPU regions
  • Creates three semaphores
  • Ping and pong tasks signal each other using semaphores and task notifications
  • Creates 2 HW ISR and ping/pong task is signaled from the ISR
  • Ping/Pong tasks increment a global ping/pong counter as well as a shared counter in between task switch

Following tables summaries relevant memory map used by the example along with the static MPU regions configurations as well as the task specific MPU regions configurations,

Memory Section Origin Size Static MPU Region Mapping Dynamic MPU Region Mapping
R5F_VECS 0x00000000 64 B [1]ATCM -
R5F_TCMA 0x00000040 31.9 KB [1]ATCM -
R5F_TCMB 0x00080000 32 KB [2]BTCM -
FLASH 0x60100000 512 KB [6]FLASH -
SBL 0x70000000 256 KB [3]OCRAM_BACKGROUND -
OCRAM 0x70040000 128 KB [4]OCRAM_UNPRIVILEGED -
PRIVILEGED_TEXT 0x70060000 64 KB [5]OCRAM_PRIVILEGED_TEXT -
PRIVILEGED_DATA 0x70070000 56 KB [3]OCRAM_BACKGROUND [8]Ping/Pong Task Stack Region
PING_TEXT 0x7007E000 2 KB [3]OCRAM_BACKGROUND [9]Ping Task Region 0
PING_DATA 0x7007E800 2 KB [3]OCRAM_BACKGROUND [10]Ping Task Region 1
PONG_TEXT 0x7007F000 2 KB [3]OCRAM_BACKGROUND [9]Pong Task Region 0
PONG_DATA 0x7007F800 2 KB [3]OCRAM_BACKGROUND [10]Pong Task Region 1
[idx]Static MPU Regions Base Address Size Execute Access Permissions
[0]BACKGROUND_REGION 0x00000000 2 GB No Supervisor RW, User RW
[1]ATCM 0x00000000 32 KB Yes Supervisor RW, User BLOCK
[2]BTCM 0x00080000 32 KB Yes Supervisor RW, User BLOCK
[3]OCRAM_BACKGROUND 0x70000000 2 MB No Supervisor RW, User BLOCK
[4]OCRAM_UNPRIVILEGED 0x70040000 128 KB Yes Supervisor RW, User RW
[5]OCRAM_PRIVILEGED_TEXT 0x70060000 64 KB Yes Supervisor RD, User BLOCK
[6]FLASH 0x60100000 512 KB Yes Supervisor RD, User BLOCK
[idx]Ping/Pong Task MPU Regions Base Address Size Execute Access Permissions
[8]Stack Region - - No Supervisor RW, User RW
[9]PING_TEXT/PONG_TEXT 0x7007E000/0x7007F000 *2 KB Yes Supervisor RD, User RD
[10]PING_DATA/PONG_DATA 0x7007E800/0x7007F800 *2 KB No Supervisor RW, User RW

Note:

  • [0]BACKGROUND_REGION with User RW access is required for peripheral access
  • [3]OCRAM_BACKGROUND maps entire OCRAM memory as Supervisor R/W only, restricting access by User
    • Other overlay regions to give only the required access to user
  • [8]Stack Region base address and size is dynamic
    • MPU entry is added using the the stack buffer address and size
  • [9]PING_TEXT/PONG_TEXT and [10]PING_DATA/PONG_DATA size is based on actual usage
    • MPU entry is added using the linker script variables

The example source files are split to dedicated files to achieve following access restrictions,

  • All text and data in task_switch_mpu.c is by default placed in privileged functions and privileged data sections respectively with following in linker script:-
    .text.task_switch_mpu.privileged : {
    task_switch_mpu.obj(.text)
    } palign(8)
    } > PRIVILEGED_TEXT
    .data.task_switch_mpu.privileged : {
    task_switch_mpu.obj(.data, .bss)
    } palign(8)
    } > PRIVILEGED_DATA
    Hence user mode tasks won't have access to any of the text/data in task_switch_mpu.c. Ping/Pong task stacks are defined in task_switch_mpu.c and will be placed in privileged data section. But as part of user task creation a dedicated MPU region will be configured for the task stack.
  • All text and data in task_switch_mpu_ping.c is by default placed in corresponding sections reserved for the ping task with the following in linker script:-
    GROUP : {
    .text.task_switch_mpu.ping : {
    task_switch_mpu_ping.obj(.text)
    } palign(8)
    } > PING_TEXT
    RUN_START(__TEXT_PING_START)
    RUN_END(__TEXT_PING_END)
    GROUP : {
    .data.task_switch_mpu.ping : {
    task_switch_mpu_ping.obj(.data, .bss)
    } palign(8)
    } > PING_DATA
    RUN_START(__DATA_PING_START)
    RUN_END(__DATA_PING_END)
    The linker variables __TEXT_PING_START, __TEXT_PING_END, __DATA_PING_START, __DATA_PING_END will be used to create the MPU regions for the ping task. Hence other user mode tasks won't have access to any of the text/data in task_switch_mpu_ping.c.
  • All text and data in task_switch_mpu_pong.c is by default placed in corresponding sections reserved for the pong task with the following in linker script:-
    GROUP : {
    .text.task_switch_mpu.pong : {
    task_switch_mpu_pong.obj(.text)
    } palign(8)
    } > PONG_TEXT
    RUN_START(__TEXT_PONG_START)
    RUN_END(__TEXT_PONG_END)
    GROUP : {
    .data.task_switch_mpu.pong : {
    task_switch_mpu_pong.obj(.data, .bss)
    } palign(8)
    } > PONG_DATA
    RUN_START(__DATA_PONG_START)
    RUN_END(__DATA_PONG_END)
    The linker variables __TEXT_PONG_START, __TEXT_PONG_END, __DATA_PONG_START, __DATA_PONG_END will be used to create the MPU regions for the pong task. Hence other user mode tasks won't have access to any of the text/data in task_switch_mpu_pong.c.
  • All text and data in task_switch_mpu_common.c is by default placed in generic text and data segments in OCRAM which falls under OCRAM_UNPRIVILEGED MPU region configuration. These will be accessible by user mode tasks unless explicitly specified by an attribute to place in a different dedicated section with reduced access permissions.
    • Same is the case with SDK driver APIs and data.
  • In summary,
    • Any text/data which is not required by user mode tasks is placed in task_switch_mpu.c
    • Any text/data which is required only by ping task is placed in task_switch_mpu_ping.c
    • Any text/data which is required only by pong task is placed in task_switch_mpu_pong.c
    • Any text/data which is required by both ping & pong tasks is placed in task_switch_mpu_common.c

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos_mpu
Toolchain ti-arm-clang
Boards am261x-som, am261x-lp
Example folder examples/kernel/freertos/task_switch_mpu

Steps to Run the Example

See Also

FreeRTOS

Sample Output

Shown below is a sample output when the application is run,

FreeRTOS MPU Task Switch example ... start !!!
[FreeRTOS] ping task ... start !!!
Performing task switch using semaphores
pong count = 100000
ping count = 100000
common count = 200000
execution time for task switches = 1706467 us
number of task switches = 200000
time per task switch (semaphore give/take) = 8532 ns
Performing task switch using direct-to-task notification
pong count = 100000
ping count = 100000
common count = 200000
execution time for task switches = 1509621 us
number of task switches = 200000
time per task switch (direct-to-task notification give/take) = 7548 ns
Performing task switch using interrupts
pong count = 100000
ping count = 100000
common count = 200000
execution time for task - ISR - task - task switches = 1652114 us
number of ISRs = 200000
time per task - ISR - task switch (semaphore give/take) = 8260 ns
[FreeRTOS] ping task ... done !!!
All tests have passed!!