AM261x MCU+ SDK  26.00.00
Driver Porting Layer (DPL) Low Latency Interrupt

Introduction

This examples demonstrates the performance and features of optimized R5F IRQ handler in DPL of MCU_PLUS_SDK

  • Part 1 demonstrates Interrupt Latency
  • Part 2 demsontrates Nesting/Re-entrancy support and floating point (FPU) save/restore support

Also refer Performance Optimizations Guide

Block diagram and expected output

Flow chart

This example uses following assembly macros for IRQ handling. These are defined in the mcu_plus_sdk\source\kernel\nortos\dpl\r5\HwiP_armv7r_vim.h file

  • ISR_CALL_LEVEL_NONFLOAT_NONREENTRANT and ISR_CALL_PULSE_NONFLOAT_NONREENTRANT
    • Use this if nesting of another interrupt inside this IRQ handler is not required and R5F Floating Point Unit is not used inside user ISR code
  • ISR_CALL_LEVEL_FLOAT_NONREENTRANT and ISR_CALL_PULSE_FLOAT_NONREENTRANT
    • Use this if nesting of another interrupt inside this IRQ handler is not required and R5F Floating Point Unit is used inside user ISR code
  • ISR_CALL_LEVEL_NONFLOAT_REENTRANT and ISR_CALL_PULSE_NONFLOAT_REENTRANT
    • Use this if nesting of another interrupt inside this IRQ handler is required and R5F Floating Point Unit is not used inside user ISR code
  • ISR_CALL_LEVEL_FLOAT_REENTRANT and ISR_CALL_PULSE_FLOAT_REENTRANT
    • Use this if nesting of another interrupt inside this IRQ handler is required and R5F Floating Point Unit is used inside user ISR code
  • ISR_CALL_PULSE_FLOAT_SELF_REENTRANT
    • Use this if nesting of same interrupt inside this IRQ handler is required and R5F Floating Point Unit is used inside user ISR code
    • Supports self-nesting
  • ISR_CALL_PULSE_NONFLOAT_SELF_REENTRANT
    • Use this if nesting of same interrupt inside this IRQ handler is required and R5F Floating Point Unit is not used inside user ISR code
    • Supports self-nesting

Refer the page Optimize Interrupt handling (IRQ/FIQ) for steps to register custom interrupt using above macros and expected latency (cycles) improvements.

Benchmarks:

  • Refer table below for measurement of execution time of Interrupt handler (NORTOS, IRQ handlers)
  • These measurements include IRQ entry handling latency + EPWM interrupt clear + IRQ exit handling latency + GPIO toggling overheads in background task
Interrupt handler Measured execution time
1. Non Re-entrant, Without FPU context save 310ns
2. Non Re-entrant, With FPU context save 426ns
3. Re-entrant, Without FPU context save 376ns
4. Re-entrant, With FPU context save 496ns

Supported Combinations

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Establish the specified external hardware connections.
  • Observe the logs printed on the console.

External connections required

See Also

Driver Porting Layer (DPL)

Sample Output

Shown below is a sample output when the application is run,

DPL Low latency interrupt example started...
Interrupt Latency test...
Configuring source of interrupts... Done.
Registering interrupt handler in R5F VIM... Done.
Configuring pin to toggle in background loop... Done.
Please observe pin (GPIO 43)
If toggling -> Background loop running
If gap/no toggling -> Background loop interrupted. Interrupt routine running
Waiting for few seconds... Done.
De-initializations... Done.
Nesting and float point context save test...
Configuring source of interrupts... Done.
Registering interrupt handlers in R5F VIM... Done.
Configuring pins to use in interrupt routine... Done.
Please observe pins (GPIO 44 and 45)
If pin 44 high -> ISR 1 running
If pin 45 high -> ISR 2 running
Waiting for few seconds...
De-initializations... Done.
All tests have passed!!

Sample output