AM261x MCU+ SDK  26.00.00
SDFM ECAP Loop Back Example

Introduction

Example Block diagram

Example Description

ECAP in its APWM mode can be used a Clock for the SDFM. This example demonstrates the configurations and usage of such internal loopback. In AM263Px, the loopback configurations can be done to leverage the following pairs.

SDFM instance Clock ECAP instances
0 0 0(default), 7
0 1 1(default), 6
0 2 2(default), 5
0 3 3(default), 4
1 0 4(default), 3
1 1 5(default), 2
1 2 6(default), 1
1 3 7(default), 0

In this example, SDFM filters 2,3 are configured for the clock input to have from filter 1 and filter 1 is configured to take the loopback clock. The Data interrupts from the SDFM filter 2,3 invoke the ISR, where the CPU reads the data form FIFO of Filter 2 and Data result of Filter 3.

Configurations

SDFM configuration is shown below:

  • SDFM used in this example - SDFM0
  • Input control mode selected - MODE0
  • Data filter settings
    • filters 2,3 modules enabled
    • Sinc1 filter selected
    • OSR = 256
    • All the filters are synchronized by using MFE (Main Filter enable bit)
    • Filter output represented in 16 bit format
  • Interrupt module settings for SDFM filter
    • FIFO full interrupt from Filter 2 and Data ready from Filter 3 are enabled.

External Connections

  • Connect Sigma-Delta data streams to SDFM0_D1, SDFM0_D2
  • Output xbar out 8 or SDFM0_CLK0 can be used for providing clock to external sdfm modulator.

AM263PX-CC (E2) with 180 pin HSEC Dock

  • SDFM0_CLK0 can be probed at HSEC Pin 72 for Clock
  • OutputXbar8 can be probed at HSEC Pin 85 for Clock
  • Provide Data Streams on SDFM0_D1 at HSEC 99 or, alternately, use EPWM0_A output for data stream input from HSEC 49
  • Provide Data Streams on SDFM0_D2 at HSEC 103 or, alternately, use EPWM0_A output for data stream input from HSEC 49

AM263PX-LP (E2)

Not Supported

AM261X-SOM (E1) with 180 pin HSEC Dock

  • SDFM1_CLK0 can be probed at HSEC Pin 100 for Clock
  • OutputXbar5 can be probed at HSEC Pin 76 for Clock
  • Provide Data Streams on SDFM1_D1 at HSEC 106 or, alternately, use EPWM0_A output for data stream input from HSEC 49
  • Provide Data Streams on SDFM1_D2 at HSEC 153 or, alternately, use EPWM0_A output for data stream input from HSEC 49

AM261X-LP Rev A

  • SDFM1_CLK0 can be probed at J1/3 pin 6 (needs IO Expander to demux from ADC input) otherwise, probe the output clock at the outputxbar output (see below).
  • OutputXbar5 can be probed at J5/7 48 for the ECAP generated Clock Source which is internally fed to the SDFM instance.
  • Provide Data Streams on SDFM1_D1 at J6/8 59 or, alternately, use EPWM2_A output for data stream input from J2/4 40
  • Provide Data Streams on SDFM1_D2 at J6/8 54 or, alternately, use EPWM2_A output for data stream input from J2/4 40

Watch Variables

  • filter2Result - Output of filter 2
  • filter3Result - Output of filter 3

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am261x-som
Example folder examples/drivers/sdfm/sdfm_ecap_loop_back/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the UART console logs for results

See Also

SDFM

Sample Output

Shown below is a sample output when the application is run,

SDFM filter sync CPU read Test Started ...
Max Samples read complete. Printing some of the values...
Filter out :
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Corresponding FIFO DATA
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Filter out :
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Corresponding FIFO DATA
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Filter out :
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Corresponding FIFO DATA
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Filter out :
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Corresponding FIFO DATA
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Filter out :
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Corresponding FIFO DATA
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Filter out :
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
Corresponding FIFO DATA
256 256 256 256 256 256 256 256 256 256 256 256 256 256 256 256
All tests have passed!!