AM261x MCU+ SDK  26.00.00
OSPI Flash DMA LLD

Introduction

This example demonstrates the OSPI low latency transfer using DMA. 16 bytes of known data are written to the flash. This data is then read back ten times by adjusting the TRPD for infinite TR reload. By this way the read can be done with really low latencies. The read back data is then compared with the known, sent data.

The average time for transfers is then printed out, and if all transfers were successful, the test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am261x-som, am261x-lp
Example folder examples/drivers/ospi/ospi_flash_diag_lld

Steps to Run the Example

See Also

OSPI

Sample Output

All tests have passed !!!