AM261x MCU+ SDK  26.00.00
OSPI Dual Flash IO

Introduction

This example demonstrates basic read write to both of the OSPI flash instances configured in polled mode of operation. APIs from flash driver are used to read and write to both the flashes. The underlying OSPI reads and writes are taken care by the flash APIs.

The example writes known data to a particular offset in the flashes and then reads it back. The read back data is then compared with the written known data.

When the comparisons match on both the flash read's, test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am261x-som, am261x-lp
Example folder examples/drivers/ospi/ospi_dual_flash_io

Steps to Run the Example

See Also

OSPI

Sample Output

All tests have passed!!