AM261x MCU+ SDK  26.00.00
I2C Led Blink

Introduction

This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.

Application exits after 10 iterations..

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
iar-arm
Board am261x-lp, am261x-som
Example folder examples/drivers/i2c/i2c_led_blink/

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

I2C LED Blink Test Started ...
LED will Blink for 10 loop ...
I2C LED Blink Test Passed!!
All tests have passed!!