AM261x MCU+ SDK  26.00.00
EDMA MultiMem Transfer

Introduction

This example demonstrates the data transfer using EDMA between different memories in the SOC. It also prints out the time taken for each transfer.

Supported Combinations

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[Cortex_R5_0] [EDMA] Interrupt Transfer Test Started...
[EDMA MULTIMEM TRANSFER] OCRAM to OCRAM Total transfer time for 1KB = 52 usecs
[EDMA MULTIMEM TRANSFER] TCMA to TCMA Total transfer time for 1KB = 47 usecs
[EDMA MULTIMEM TRANSFER] TCMB to TCMB Total transfer time for 1KB = 48 usecs
[EDMA MULTIMEM TRANSFER] OCRAM to TCMA Total transfer time for 1KB = 47 usecs
[EDMA MULTIMEM TRANSFER] TCMA to OCRAM Total transfer time for 1KB = 49 usecs
[EDMA] Interrupt Transfer Test Completed!!
All tests have passed!!