|
AM261x MCU+ SDK
26.00.00
|
|
Introduction
- CPSW operates in two modes
- Switch Mode - packet forwarding is enabled and packets are forwarded to Host + Other MAC ports. This is the default configuration for CPSW.
- MAC mode - packets are only given to the Host port and are not forwarded to other MAC Ports.
CPSW DUAL MAC Mode
- In this mode, both the MAC ports of AM261X are configured to be in MAC mode.
- This mode requires two Network interfaces to operate.
- It is recommended to use two separate subnets for working with DUAL MAC.
- A single implementation of network interface and shared pool is used for both the Netifs.
- Dual MAC feature is illustrated by the below image:
DUAL MAC Operation
See Also
Ethernet And Networking