AM261x MCU+ SDK  11.01.00
dwc_usb3_dev_ep_regs_t Struct Reference

Detailed Description

Device Endpoint Specific Registers Offsets 800h-9ECh for OUT, 810h-9FCh for IN. There will be one set of endpoint registers per logical endpoint implemented.

Data Fields

volatile u32 depcmdpar2
 
volatile u32 depcmdpar1
 
volatile u32 depcmdpar0
 
volatile u32 depcmd
 
volatile u32 reserved [4]
 

Field Documentation

◆ depcmdpar2

volatile u32 dwc_usb3_dev_ep_regs_t::depcmdpar2

Device Endpoint Command Parameter 2 Register Offset: 800h/810h + (ep_num * 20h) + 00h

◆ depcmdpar1

volatile u32 dwc_usb3_dev_ep_regs_t::depcmdpar1

Device Endpoint Command Parameter 1 Register Offset: 800h/810h + (ep_num * 20h) + 04h

◆ depcmdpar0

volatile u32 dwc_usb3_dev_ep_regs_t::depcmdpar0

Device Endpoint Command Parameter 0 Register Offset: 800h/810h + (ep_num * 20h) + 08h

◆ depcmd

volatile u32 dwc_usb3_dev_ep_regs_t::depcmd

Device Endpoint Command Register Offset: 800h/810h + (ep_num * 20h) + 0Ch. Fields defined in enum depcmd_data.

◆ reserved

volatile u32 dwc_usb3_dev_ep_regs_t::reserved[4]

reserved Offset: 800h/810h + (ep_num * 20h) + 10h-1Ch