AM261x MCU+ SDK  11.01.00
dwc_usb3_core_params_t Struct Reference

Detailed Description

These parameters may be specified when loading the module. They define how the DWC_usb3 controller should be configured. The parameter values are passed to the CIL initialization routine dwc_usb3_pcd_common_init().

Data Fields

int burst
 
int newcore
 
int phy
 
int wakeup
 
int pwrctl
 
int lpmctl
 
int phyctl
 
int usb2mode
 
int hibernate
 
int hiberdisc
 
int clkgatingen
 
int ssdisquirk
 
int nobos
 
int loop
 
int nump
 
int newcsr
 
int rxfsz
 
int txfsz [16]
 
int txfsz_cnt
 
int baseline_besl
 
int deep_besl
 
int besl
 

Field Documentation

◆ burst

int dwc_usb3_core_params_t::burst

◆ newcore

int dwc_usb3_core_params_t::newcore

◆ phy

int dwc_usb3_core_params_t::phy

◆ wakeup

int dwc_usb3_core_params_t::wakeup

◆ pwrctl

int dwc_usb3_core_params_t::pwrctl

◆ lpmctl

int dwc_usb3_core_params_t::lpmctl

◆ phyctl

int dwc_usb3_core_params_t::phyctl

◆ usb2mode

int dwc_usb3_core_params_t::usb2mode

◆ hibernate

int dwc_usb3_core_params_t::hibernate

◆ hiberdisc

int dwc_usb3_core_params_t::hiberdisc

◆ clkgatingen

int dwc_usb3_core_params_t::clkgatingen

◆ ssdisquirk

int dwc_usb3_core_params_t::ssdisquirk

◆ nobos

int dwc_usb3_core_params_t::nobos

◆ loop

int dwc_usb3_core_params_t::loop

◆ nump

int dwc_usb3_core_params_t::nump

◆ newcsr

int dwc_usb3_core_params_t::newcsr

◆ rxfsz

int dwc_usb3_core_params_t::rxfsz

◆ txfsz

int dwc_usb3_core_params_t::txfsz[16]

◆ txfsz_cnt

int dwc_usb3_core_params_t::txfsz_cnt

◆ baseline_besl

int dwc_usb3_core_params_t::baseline_besl

◆ deep_besl

int dwc_usb3_core_params_t::deep_besl

◆ besl

int dwc_usb3_core_params_t::besl