|
AM261x MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
34 #ifndef SDL_MCU_ARMSS_CCMR5_H
35 #define SDL_MCU_ARMSS_CCMR5_H
41 #include "sdlr_mcu_armss_ccmr5.h"
80 typedef enum SDL_McuArmssCcmR5RegId_e
96 #
if defined (SOC_AM263PX) || (SOC_AM261X)
97 SDL_MCU_ARMSS_CCMR5_CCMKEYR5_REGID = (7u),
99 SDL_MCU_ARMSS_CCMR5_CCMSR5_REGID = (8u),
101 SDL_MCU_ARMSS_CCMR5_CCMKEYR6_REGID = (9u),
103 SDL_MCU_ARMSS_CCMR5_CCMSR6_REGID = (10u),
120 typedef enum SDL_McuArmssCcmR5ModuleId_e
128 #
if defined (SOC_AM263PX) || (SOC_AM261X)
129 SDL_MCU_ARMSS_CCMR5_TMU_MODULE_ID = (3u),
131 SDL_MCU_ARMSS_CCMR5_RL2_MODULE_ID = (4u),
149 typedef enum SDL_McuArmssCcmR5OpModeKey_e
187 uintptr_t baseAddress,
189 uint32_t *pValToBeRead,
211 uintptr_t baseAddress,
213 uint32_t valToBeWritten,
236 uintptr_t baseAddress,
261 uintptr_t baseAddress,
299 uintptr_t baseAddress,
323 uintptr_t baseAddress,
@ SDL_MCU_ARMSS_CCMR5_CCMSR3_REGID
Definition: sdl_mcu_armss_ccmr5.h:90
@ SDL_MCU_ARMSS_CCMR5_INVALID_MODULE_ID
Definition: sdl_mcu_armss_ccmr5.h:134
@ SDL_MCU_ARMSS_CCMR5_CCMKEYR2_REGID
Definition: sdl_mcu_armss_ccmr5.h:88
@ SDL_MCU_ARMSS_CCMR5_VIM_MODULE_ID
Definition: sdl_mcu_armss_ccmr5.h:124
@ SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_MODE
Definition: sdl_mcu_armss_ccmr5.h:153
@ SDL_MCU_ARMSS_CCMR5_CCMSR1_REGID
Definition: sdl_mcu_armss_ccmr5.h:82
@ SDL_MCU_ARMSS_CCMR5_INACTIVITY_MONITOR_MODULE_ID
Definition: sdl_mcu_armss_ccmr5.h:126
SDL_McuArmssCcmR5ModuleId
This enum defines the MCU ARMSS CCM R5 module ID type used under the context of SDL CCMR5 APIs.
Definition: sdl_mcu_armss_ccmr5.h:121
@ SDL_MCU_ARMSS_CCMR5_CPU_MODULE_ID
Definition: sdl_mcu_armss_ccmr5.h:122
@ SDL_MCU_ARMSS_CCMR5_MKEY_CMP_MODE_ACTIVE
Definition: sdl_mcu_armss_ccmr5.h:151
@ SDL_MCU_ARMSS_CCMR5_MKEY_ERR_FORCE_MODE
Definition: sdl_mcu_armss_ccmr5.h:155
SDL_McuArmssCcmR5RegId
This typedef defines the MCU ARMSS CCM R5 register ID type used under the context of SDL CCMR5 APIs.
Definition: sdl_mcu_armss_ccmr5.h:81
@ SDL_MCU_ARMSS_CCMR5_CCMKEYR3_REGID
Definition: sdl_mcu_armss_ccmr5.h:92
int32_t SDL_armR5CCMClearCompareError(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, int32_t *pMetaInfo)
Clear Compare Error value for CPU, VIM, CCM Inactivity monitor.
SDL_McuArmssCcmR5OpModeKey
This enum defines the MCU ARMSS CCM R5 Operation Mode Key values used under the context of SDL CCMR5 ...
Definition: sdl_mcu_armss_ccmr5.h:150
@ SDL_MCU_ARMSS_CCMR5_CCMSR2_REGID
Definition: sdl_mcu_armss_ccmr5.h:86
int32_t SDL_armR5CCMGetOperationModeKey(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey *pOpModeKey, int32_t *pMetaInfo)
Get Operation mode key value for CPU, VIM, CCM Inactivity monitor.
int32_t SDL_armR5ConfigureCCMRegister(uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t valToBeWritten, int32_t *pMetaInfo)
Configure CCM Regiser.
@ SDL_MCU_ARMSS_CCMR5_POLCNTRL_REGID
Definition: sdl_mcu_armss_ccmr5.h:94
int32_t SDL_armR5CCMSetOperationModeKey(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, SDL_McuArmssCcmR5OpModeKey opModeKey, int32_t *pMetaInfo)
Configure Operating mode for CPU, VIM, CCM Inactivity monitor.
@ SDL_MCU_ARMSS_CCMR5_INVALID_REGID
Definition: sdl_mcu_armss_ccmr5.h:106
int32_t SDL_armR5ReadCCMRegister(uintptr_t baseAddress, SDL_McuArmssCcmR5RegId regId, uint32_t *pValToBeRead, int32_t *pMetaInfo)
Read CCM Regiser.
@ SDL_MCU_ARMSS_CCMR5_CCMKEYR1_REGID
Definition: sdl_mcu_armss_ccmr5.h:84
int32_t SDL_armR5CCMGetCompareError(uintptr_t baseAddress, SDL_McuArmssCcmR5ModuleId moduleId, uint32_t *pCmpError, int32_t *pMetaInfo)
Read Compare Error status for CPU, VIM, CCM Inactivity monitor.
@ SDL_MCU_ARMSS_CCMR5_MKEY_SELF_TEST_ERR_FORCE_MODE
Definition: sdl_mcu_armss_ccmr5.h:157