AM261x MCU+ SDK  11.01.00

Introduction

Data Structures

struct  SDL_PBIST_config
 This structure contains the different configuration used for PBIST. More...
 
struct  SDL_PBIST_configNeg
 This structure contains the different configuration used for PBIST for the failure insertion test to generate negative result. More...
 

Functions

int32_t SDL_PBIST_softReset (SDL_pbistRegs *pPBISTRegs)
 PBIST Soft reset. More...
 
int32_t SDL_PBIST_start (SDL_pbistRegs *pPBISTRegs, const SDL_PBIST_config *pConfig)
 PBIST Start. More...
 
int32_t SDL_PBIST_startNeg (SDL_pbistRegs *pPBISTRegs, const SDL_PBIST_configNeg *pConfig)
 PBIST Failure Insertion Test Start. More...
 
int32_t SDL_PBIST_checkResult (const SDL_pbistRegs *pPBISTRegs, bool *pResult)
 PBIST check result. More...
 
int32_t SDL_PBIST_releaseTestMode (SDL_pbistRegs *pPBISTRegs)
 PBIST Release Test mode. More...
 
int32_t SDL_PBIST_Instance (SDL_PBIST_inst instance)
 PBIST Instance. More...
 

Macros

#define PBIST_MAX_NUM_RUNS   30U
 

Macro Definition Documentation

◆ PBIST_MAX_NUM_RUNS

#define PBIST_MAX_NUM_RUNS   30U

Function Documentation

◆ SDL_PBIST_softReset()

int32_t SDL_PBIST_softReset ( SDL_pbistRegs pPBISTRegs)

PBIST Soft reset.

This function resets PBIST Module. In general called before running a new test.

Parameters
pPBISTRegs[IN] Pointer to PBIST registers base
Returns
The SDL error code for the API. If pBISTRegs is NULL: SDL_EBADARGS Success: SDL_PASS

◆ SDL_PBIST_start()

int32_t SDL_PBIST_start ( SDL_pbistRegs pPBISTRegs,
const SDL_PBIST_config pConfig 
)

PBIST Start.

This function configures the paramters for PBIST and starts execution.

Parameters
pPBISTRegs[IN] Pointer to PBIST registers base
pConfig[IN] Pointer to PBIST configuration
Returns
The SDL error code for the API. If pBISTRegs or pConfig is NULL : SDL_EBADARGS Success: SDL_PASS

◆ SDL_PBIST_startNeg()

int32_t SDL_PBIST_startNeg ( SDL_pbistRegs pPBISTRegs,
const SDL_PBIST_configNeg pConfig 
)

PBIST Failure Insertion Test Start.

This function configures the parameters for PBIST Test for Diagnostics to insert a failure to generate the negative result and starts execution.

Parameters
pPBISTRegs[IN] Pointer to PBIST registers base
pConfig[IN] Pointer to PBIST configuration
Returns
The SDL error code for the API. If pBISTRegs or pConfig in NULL : SDL_EBADARGS Success: SDL_PASS

◆ SDL_PBIST_checkResult()

int32_t SDL_PBIST_checkResult ( const SDL_pbistRegs pPBISTRegs,
bool *  pResult 
)

PBIST check result.

This function checks if PBIST test has passed.

Parameters
pPBISTRegs[IN] Pointer to PBIST registers base
pResult[OUT] Pointer to variable to indicate result
Returns
The SDL error code for the API. If pBISTRegs or pResult is NULL: SDL_EBADARGS Success: SDL_PASS

◆ SDL_PBIST_releaseTestMode()

int32_t SDL_PBIST_releaseTestMode ( SDL_pbistRegs pPBISTRegs)

PBIST Release Test mode.

This function releases test mode. In general called after test is complete to switch back to normal operation.

Parameters
pPBISTRegs[IN] Pointer to PBIST registers base
Returns
The SDL error code for the API. If pBISTRegs is NULL: SDL_EBADARGS Success: SDL_PASS

◆ SDL_PBIST_Instance()

int32_t SDL_PBIST_Instance ( SDL_PBIST_inst  instance)

PBIST Instance.

This function specifies the PBITST Instance

Parameters
instance[IN] Value of PBIST instance