AM261x MCU+ SDK  11.01.00

Introduction

These APIs try are used for the phy tuning

Functions

void OSPI_lld_Transaction_init (OSPI_Transaction *trans)
 Function to initialize the OSPI_Transaction structure. More...
 
void OSPI_lld_readCmdParams_init (OSPI_ReadCmdParams *rdParams)
 Function to initialize the OSPI_ReadCmdParams structure. More...
 

Function Documentation

◆ OSPI_lld_Transaction_init()

void OSPI_lld_Transaction_init ( OSPI_Transaction trans)

Function to initialize the OSPI_Transaction structure.

Parameters
transPointer to a OSPI_Transaction

◆ OSPI_lld_readCmdParams_init()

void OSPI_lld_readCmdParams_init ( OSPI_ReadCmdParams rdParams)

Function to initialize the OSPI_ReadCmdParams structure.

Parameters
rdParamsPointer to a OSPI_ReadCmdParams