AM261x MCU+ SDK  11.01.00

Introduction

This module contains APIs to program and use the FOTA Agent driver.

Files

file  fota_agent.h
 FOTA Agent Driver API/interface file.
 

Data Structures

struct  FOTAAgent_Params
 FOTA Agent Driver Handle. More...
 
struct  FOTAAgent_Handle
 

Functions

int32_t FOTAAgent_Params_init (FOTAAgent_Params *params)
 Initilize params with default values. More...
 
int32_t FOTAAgent_init (FOTAAgent_Handle *pHandle, FOTAAgent_Params *params)
 Initilize FOTA Agent API. More...
 
int32_t FOTAAgent_writeStart (FOTAAgent_Handle *pHandle, uint32_t wrOffset, char doFlashSegments)
 Logically start writes and initilize state internal machine. More...
 
int32_t FOTAAgent_writeUpdate (FOTAAgent_Handle *pHandle, uint8_t *buf, uint32_t size)
 Update internal machine with new data. More...
 
int32_t FOTAAgent_writeEnd (FOTAAgent_Handle *pHandle)
 Logically end writes and end the state machine. More...
 
int32_t FOTAAgent_getFLSOPSKDHandle (FOTAAgent_Handle *pHandle, FLSOPSKD_Handle *flsopskdHandle)
 Retrive FLSOPSKD handle. More...
 

Macros

#define FOTAAGENT_WRITEOFFSET_DNC   (0U)
 

Macro Definition Documentation

◆ FOTAAGENT_WRITEOFFSET_DNC

#define FOTAAGENT_WRITEOFFSET_DNC   (0U)

Function Documentation

◆ FOTAAgent_Params_init()

int32_t FOTAAgent_Params_init ( FOTAAgent_Params params)

Initilize params with default values.

Parameters
paramspointer to parameter struct
Returns
SystemP_FAILURE
SystemP_SUCCESS

◆ FOTAAgent_init()

int32_t FOTAAgent_init ( FOTAAgent_Handle pHandle,
FOTAAgent_Params params 
)

Initilize FOTA Agent API.

This API initilize FOTA agent and underneath modules.

Parameters
pHandlepointer to FOTA Agent handle
paramspointer to parameter struct
Returns
SystemP_FAILURE
SystemP_SUCCESS

◆ FOTAAgent_writeStart()

int32_t FOTAAgent_writeStart ( FOTAAgent_Handle pHandle,
uint32_t  wrOffset,
char  doFlashSegments 
)

Logically start writes and initilize state internal machine.

Currently, FOTAAgent only support binary file of format .mcelf and .mcelf_xip. if file type is mcelf_xip then doFlashSegments is TRUE else it is FALSE. doFlashSegments here signals to parse the file, extracts the data segments and only flash those data segments, instead of entire file.

In case doFlashSegments is TRUE, wrOffset argument is ignored as this information is stored inside the file. However, wrOffset information needs to be provided explicitly given via wrOffset argument.

wrOffset argument is the offset (in bytes) at which file needs to be written.

Parameters
pHandlepointer to FOTA Agent handle
wrOffsetflash offset at which file to write
doFlashSegmentsflash data segments only instead of entire file
Returns
SystemP_FAILURE
SystemP_SUCCESS

◆ FOTAAgent_writeUpdate()

int32_t FOTAAgent_writeUpdate ( FOTAAgent_Handle pHandle,
uint8_t *  buf,
uint32_t  size 
)

Update internal machine with new data.

Update internal state machine with new data. Its not that on providing every one byte this function will write to flash. Flash constraints on erase size. For exmaple, if erase is sector wise of 4096 bytes (as specified in params) then in that case, this function will wait for this amount of data to be recieved and then send it to the flash.

Parameters
pHandlepointer to FOTA Agent handle
bufpointer to buffer with the data
sizesize of buf
Returns
SystemP_FAILURE
SystemP_SUCCESS

◆ FOTAAgent_writeEnd()

int32_t FOTAAgent_writeEnd ( FOTAAgent_Handle pHandle)

Logically end writes and end the state machine.

Other than ending the internal state machine, this function will also flash any remaining data that remains to be programmed.

Parameters
pHandlepointer to FOTA Agent handle
Returns
SystemP_FAILURE
SystemP_SUCCESS

◆ FOTAAgent_getFLSOPSKDHandle()

int32_t FOTAAgent_getFLSOPSKDHandle ( FOTAAgent_Handle pHandle,
FLSOPSKD_Handle flsopskdHandle 
)

Retrive FLSOPSKD handle.

Parameters
pHandle[in] pointer to FOTA Agent handle
flsopskdHandle[out] pointer to flsopskdHandle
Returns
SystemP_FAILURE
SystemP_SUCCESS