AM261x MCU+ SDK  11.01.00
Release Notes 11.00.00

Attention
1. Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
2. RPRC image format has been deprecated from this release. Multi Core ELF image format should be used. (Understanding Multicore ELF image format).
3. DFU Utils tool is not supported on Mac systems due to a build issue.
4. SDK has been updated to support CCS Theia Out of Box from this release. Refer to Compatibility section below for changes w.r.t Eclipse.
5. The default Stack size is 16KB and Heap size 32 KB for SDK examples. This can be adjusted as per application requirement through Memory Configurator in SysCfg or by updating Linker script in case of standalone applications.
6. For customer migrating from any release before SDK 10.00.00 to 10.00.00 or any release after, "DPL CFG" module has to be added in SysCfg in order to enable interrupts during DPL initialization. This module was added in SysCfg for 10.00.00 release to allow configuring Init time Enable/Disable of interrupts for RTOS applications (Default set to enabled).
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
Clock Tree support for PLL and Peripheral clock configuration Sysconfig
CCS Theia Support CCS
Multi Core FreeRTOS IPC Example IPC
OSPI Phy Graph Plotter Example OSPI
Rev A Launchpad Support Board
Rev A SOM Support Board
Board Level Sysconfig Support Sysconfig
USB Sysconfig support Sysconfig
McSPI External Loopback Example McSPI
USB NCM Class Support USB
FreeRTOS based CDC Example USB
LwIP stack upgrade to STABLE-2_2_1_RELEASE Networking
IET Feature Enablement via Syscfg-GUI Networking
XIP+RL2 support is included in Networking OOB example, referenced in EXAMPLES_ENET_LWIP_CPSW_UDPCLIENT Networking
SENT Decoder and Encoder Examples PRU-IO

Modules Not tested/supported in this release

  • MMCSD and GPMC drivers are not validated on AM261x LP or SOM Board.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM261x R5F AM261x Launchpad Rev A (referred to as am261x-lp in code).
Windows 10 64b or Ubuntu 18.04 64b or MacOS
AM261x R5F AM261x SOM Rev A (referred to as am261x-som in code).
Windows 10 64b or Ubuntu 18.04 64b or MacOS

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 20.3.0
SysConfig R5F 1.25.0 build, build 42688
TI ARM CLANG R5F 4.0.3.LTS
FreeRTOS Kernel R5F 11.1.0
LwIP R5F STABLE-2_2_1_RELEASE
Mbed-TLS R5F 2.13.1
Uniflash R5F 9.3.0

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
Ethernet MDIO with Clause 45 support Networking

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, UART. All R5F's. Multi-core ELF image format Force Dual Core Mode

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Examples: adc_soc_continuous_dma, adc_alternate_dma_trigger Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA (normal and alternate triggers), EPWM trip through PPB limit, PPB features, Burst mode, Single and Differential mode, Interrupt with Offset from Aquisition Window, EPWM/ECAP/RTI triggered conversions, Trigger Repeater for Undersampling and Oversampling, Global Force on Multiple ADCs, Internal DAC Loopback to Calibration Channels, Safety Checker and Aggregator, Open Short Detection feature External channel selection
Bootloader R5F YES Yes. DMA enabled for SBL OSPI Boot modes: OSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip, digital filter, Calibration CMPSS Dac LoopBack feature
CPSW R5F YES No MAC & PHY loopback(DP83826-EVM-AM2) with RMII and MII 100Mbps , MAC & PHY loopback(DP83TG720-EVM-AM2) with RGMII 1Gbps, LWIP (DP83TG720-EVM-AM2, DP83826-EVM-AM2): Getting IP, Ping, Layer 2 MAC, Layer 2 PTP Timestamping and Ethernet CPSW Switch support, TSN stack -
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES yes. Example : ecap_edma ECAP APWM mode, PWM capture, DMA trigger in both APWM and Capture Modes, Signal Monitoring features -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking, Error Handling -
EPWM R5F YES Yes. Example: epwm_dma, epwm_xcmp_dma Multiple EPWM Sync from Top Module, PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, chopper module features, type5 features, global load and link feature -
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement, speed direction, cw-ccw modes -
FSI R5F YES YES RX, TX, polling, interrupt, DMA mode, single lane loopback. - FSI Spi Mode
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
LIN R5F YES YES RX, TX, polling, interrupt, DMA mode. -
MCAN R5F YES No RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode -
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
PINMUX R5F YES NA Tested with multiple peripheral pinmuxes -
PMU R5F NO NA Tested various PMU events Counter overflow detection is not enabled
OptiFlash R5F Yes NA FLC, RL2, RAT functionality, XIP with RL2 enabled, OTFA, FOTA, Optishare, Smart Layout -
OSPI R5F YES Yes. Example: ospi_flash_dma Read direct, Write indirect, Read/Write commands, DMA for read -
RTI R5F YES No Counter read, timebase selection, comparator setup for Interrupt, DMA requests Capture feature, fast enabling/disabling of events not tested
SDFM R5F YES No ECAP Clock LoopBack, Filter data read from CPU, Filter data read with PWM sync, triggered DMA read from the Filter FIFO -
SOC R5F YES NA Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation -
SPINLOCK R5F NA NA Lock, unlock HW spinlock -
UART R5F YES Yes. Example: uart_echo_dma Basic read/write at baud rate 115200, polling, interrupt mode HW flow control not tested, DMA mode not supported
USB R5F No NA DFU, CDC Echo mode -
WATCHDOG R5F YES NA Reset mode, Interrupt mode -

Trigonometric Operations

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
TMU R5F NO NA TMU Operations, Pipelining, Contex Save Square Root, Division Operations. more than 1 Interrupt Nesting for the contex save is not Supported.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
FLASH R5F YES OSPI Flash -
LED R5F YES GPIO -
ETHPHY R5F YES Tested with ethercat_slave_beckhoff_ssc_demo example -
IOEXPANDER R5F YES IO configurability -
PMIC R5F YES Watchdog Reset and disable -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Time-Sensitive Networking(gPTP-IEEE 802.1AS) R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, scatter-gather Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC & PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer and Classifier MII mode
ICSS-EMAC R5F YES FreeRTOS Switch and MAC features, Storm Prevention (MAC), Host Statistics, Multicast Filtering Promiscuous Mode

Safety Diagnostic Library

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
MCRC R5F NA NORTOS Full CPU, Auto CPU Mode and Semi CPU Auto Mode -
DCC R5F NA NORTOS Single Shot and Continuous modes -
PBIST R5F NA NORTOS Memories supported by MSS PBIST controller. -
ESM R5F NA NORTOS Tested in combination with RTI, DCC -
RTI R5F NA NORTOS WINDOWSIZE_100_PERCENT, WINDOWSIZE_50_PERCENT ,Latency/Propagation timing error(early)(50% window),Latency/Propagation timing error(late)(50% window) -
ECC R5F NA NORTOS ECC of MSS_L2, R5F TCM, MCAN, VIM, ICSSM, TPTC FSS FOTA and OSPI
ECC Bus Safety R5F NA NORTOS AHB, AXI, TPTC -
CCM R5F NA NORTOS CCM Self Test Mode,Error Forcing Mode and Self Test Error Forcing Mode. TMU and RL2 are also validated -
R5F STC(LBIST), Static Register Read R5F NA NORTOS STC of R5F, R5F CPU Static Register Read -
TMU ROM Checksum R5F NA NORTOS ROM checksum for TMU -
Time out Gasket(STOG) R5F NA NORTOS Timeout gasket feature -
Thermal Monitor(VTM) R5F NA NORTOS Over, under and thershold temperature interrupts -
Integrated Example R5F NA FreeRTOS Integrated example with all the SDL modules integrated in to one example. ECC for TPTC, ECC Bus Safety and STC.

Note: SDL is validated only on SOM Board.

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-14055 SBL DFU and SBL DFU Uniflash Example failure USB 10.00.01 onwards AM261x Resolved in driver
MCUSDK-14502 PMIC WDG QA Example not working on AM261x-LP E2 board PMIC 10.02.00 onwards AM261x Fixed in driver by increasing sleep time for waiting to trigger wdg reset
MCUSDK-14547 XIP Flashing not supported in SBL JTAG Uniflash example SBL 10.00.00 onwards AM263Px, AM261x Added XIP flashing support in the example
MCUSDK-14609 FOTA Example Failure on AM261x SOM OptiFlash 10.02.00 onwards AM261x Resolved by reducing OSPI clock frequency from 166Mhz to 133Mhz
MCUSDK-14606 USB Enumeration fails randomly USB 10.02.00 onwards AM261x -
MCUSDK-14704 Adding multiple instances of UART DMA LLD causes failure UART 10.02.00 onwards AM263x, AM263Px, AM261x Fixed array indexing while assigning dma config
MCUSDK-14917 "Selected mode" in pinmux.csv.xdt file not being updated correctly in SysCfg Pinmux 10.01.00 onwards AM263x, AM263Px, AM261x Fixed in Pinmux CSV template
PROC_SDL-9179 Redefinition error in MCU_PBIST Sysconfig SDL 10.02.00 onwards AM263Px, AM261x Resolved in Source code
MCUSDK-14749 McSPI: Non Powers of 2 cannot be configured as fifo trigger levels in polling and interrupt mode McSPI 10.02.00 onwards AM263x, AM263Px, AM261x Fix in SysCfg Meta file.
MCUSDK-13966 All UART triggers levels not exposed in SysCfg UART 10.00.00 onwards AM263x, AM263Px, AM261x Update SysCfg to show all trigger levels from 1 to 64.
MCUSDK-14573 Incorrect handling of errata i2310 in UART isr UART 10.00.00 onwards AM263x, AM263Px, AM261x Reorder the ISR state machine for handling UART errata correctly.
MCUSDK-14706 GPIO Qual selection API missing GPIO 10.00.00 onwards AM263x, AM263Px, AM261x Qual sel API added in pinmux driver
MCUSDK-14569 UART Errata i2310 is missing a step UART 10.00.00 onwards AM263x, AM263Px, AM261x Added IIR register read to clear the interrupt
MCUSDK-14620 SDK build fails in Mac Machines Build 10.02.00 onwards AM263x, AM263Px, AM261x Added GMAC library for MAC into SDK
MCUSDK-14659 Incorrect RTI clock source mux address for RTI 4 to 7 RTI 10.00.00 onwards AM263Px, AM261x Updated to correct mux addresses in SysCfg
MCUSDK-13182 SysCfg unexpectedly changes OSPI Pin OSPI 10.00.00 onwards AM263Px, AM261x The OSPI pins are locked in SDK examples.
MCUSDK-14857, MCUSDK-14731 Core 1 unhalted in SBL before FSM Trigger, Memory load SBL 10.00.00 onwards AM263x, AM263Px, AM261x Skip unhalting core 1 of both clusters in dual core mode
MCUSDK-14712 OSPI Reset Pin being used before configuration OSPI 10.00.00 onwards AM263Px, AM261x Configure OSPI reset in OSPI open instead of Flash open
PROC_SDL-9160 PBIST does not cover the VIM memories SDL 10.02.00 onwards AM263x, AM263Px, AM261x Fixed in Source and Used polling method instead of ISR to cover VIM memory
PROC_SDL-9154 VTM Example stuck in UC2 SDL 10.02.00 onwards AM263Px, AM261x Fixed in example
MCUSDK-14695 SDFM_configComparator has incorrect input in examples SDFM 10.00.00 onwards AM263x, AM263Px, AM261x Updated example to pass correct value
MCUSDK-14696 ADC Sysconfig does not seem to generate codes for repeaters ADC 10.00.00 onwards AM263Px, AM261x Fixed syscfg template file to generate trigger repeater code for burst mode
MCUSDK-14645 Implementation of the ADC_selectSOCExtChannel ADC 10.01.00 onwards AM263Px, AM261x Fixed ADC_selectSOCExtChannel API implementation
PROC_SDL-9147 VTM Usecase stuck in integrated example SDL 10.02.00 onwards AM263Px, AM261x Fixed in integrated example

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-14148 AM261x : ZNC : Package in the early samples has ADC issue. Needs SW checks undone for ADC ADC 10.00.00 onwards Details : ZNC package currently (Jan 2025), has, ADC 0 Reference lines not connected with that of the ADC 1's. There are some packages were shipped with the ADC Reference Monitor checks are Bypassed for the ADC front end enablement in the EFUSE. the SW code gen from the syscfg will assert the ADC init if the monitor throws a fault. It is requested to bypass the SW check as well to enable the customer to use the ADC.
Workaround : only applicable in the devices with forementioned conditions.
1. Go to the file
source/sysconfig/drivers/.meta/soc_ctrl/templates/soc_ctrl_adc_config.c.xdt

2. Find line with
DebugP_assert(SOC_getAdcReferenceStatus(`montior2AdcMap[monitor][0]`) == true);

3.Change it to
//DebugP_assert(SOC_getAdcReferenceStatus(`montior2AdcMap[monitor][0]`) == true);
MCUSDK-13865 HRPWM Deadband sfo example has 1ns jitter EPWM 10.00.00 onwards -
MCUSDK-13847 AM261x: GPTP lwIP debug example doesnt fit in RAM Networking 10.00.01 onwards -
MCUSDK-13513 AM263Px, AM261x: UDP IPERF TX is unstable with 100Mbps link speed Networking 10.00.01 onwards -
MCUSDK-14950 AM26x: Networking examples show up as "..." on TIREX Networking 10.01.00 onwards -
MCUSDK-14692 Raw HTTP Server example does not work with Static IP Networking 10.02.00 onwards -
MCUSDK-14792 AM261x LwIP ping app does not work (enet_lwip_cpsw) Networking 10.02.00 onwards -
MCUSDK-13896 Syscfg does not let you configure ethernet interfaces pinmux independently Networking 10.02.00 onwards -
MCUSDK-15051 ENET: am261x: UDP client example not working in CCS boot mode Networking 11.00.00 onwards -
PINDSW-7715 Dual EMAC instance not working with both ports together for icss_emac_lwip example ICSS-EMAC 10.00.01 onwards None
PINDSW-7746 Low iperf values in TCP and UDP ICSS-EMAC 10.00.01 onwards None
PINDSW-8118 Enabling DHCP mode in icss_emac_lwip example causes assert ICSS-EMAC 10.00.01 onwards None
MCUSDK-13201 HRPWM waveform not generating (in updwon count) when prescaler is non-zero and HRPE is enabled EPWM 10.00.01 onwards None
MCUSDK-13834 EQEP: EQEP frequency measurement example is not working as expected EQEP 10.00.01 onwards None
MCUSDK-14059 CMPSS DE example has Glitch in PWM output CMPSS 10.00.01 onwards None
PROC_SDL-8392 In ECC bus safety example, ECC error is not properly cleared at the source. SDL 10.02.00 onwards None
PROC_SDL-8787 ECC TPTC and STC examples are not supported in SDL integrated example. SDL 10.02.00 onwards Use standalone examples.
PROC_SDL-8857 SDL integrated example does not support ECC Bus Safety. SDL 10.02.00 onwards Use standalone example.
PROC_SDL-9163 ECC Aggregators FSS FOTA and OSPI SDL 10.02.00 onwards None
MCUSDK-14898 SDL apps fails on other than RFSS0-0 with SBL SBL, SDL 11.00.00 onwards This because SBL brings the RFSS0-1 out of reset before the SBL UART prints gets flushed. This will be fixed in next release. As a workaround the application in R5FSS1-0 can delay the start of application till SBL UART prints gets completed.
MCUSDK-13513 Multiple chip selects cannot be configured in SysCfg OSPI 10.00.00 onwards -
MCUSDK-14582 Flash: Incorrect flash name after Loading Flash JSON OSPI 10.00.00 onwards -
MCUSDK-14613 XIP image loading not working in CCS for am261x-lp E2 board CCS, XIP 10.02.00 onwards -
MCUSDK-14714 Bufnum of 6 and 12 will cause the vring indexes to get corrupted IPC 10.00.00 onwards Use other VRING buffer numbers.
MCUSDK-14879 Potential system hang issue due to priority mask based critical sections. FreeRTOS 10.00.00 onwards Not to use Priority mask based critical sections (Disabled by default in SDK).
MCUSDK-14893 Sub projects under system projects cannot be changed in CCS Theia CCS 11.00.00 onwards -
MCUSDK-14819 Ram is getting erased/overwritten once warm reset is done in application SBL 11.00.00 onwards -
MCUSDK-14895 UART LLD Rx error checking logic checks if all errors exist at once UART 10.00.00 onwards -
MCUSDK-14613 XIP image loading not working in CCS for am261x-lp E2 board CCS, XIP 10.02.00 onwards -
MCUSDK-14647 All CANFD standard ID configurations are not exposed in syscfg gui CAN 10.02.00 onwards Configure Config type, ID's etc in application
MCUSDK-14705 Flash verify not working for XIP images Flash 10.02.00 onwards -
MCUSDK-14914 Unable to add UART communication port to target configuration in Theia Real Time Debug 10.02.00 onwards Use the CCXML file from CCS eclipse after updating to correct COM port.
MCUSDK-14941 McSPI: Non Multiple's of FIFO cannot be transferred in DMA mode McSPI 10.00.00 onwards Use FIFO Trigger level of 1.
MCUSDK-13011 Data Abort in application when all cores are running freertos using Gel files(CCS) FreeRTOS 10.00.00 onwards Flash and use SBL NULL instead of gel files
MCUSDK-14636 AM261x: Phy Tuning not supported for NAND Flash and PSRAM OSPI, Flash 10.02.00 onwards -
MCUSDK-14656 Mac OS Support not available for DFU Utils tool USB 10.02.00 onwards -
PINDSW-9499 Short serial message and enhanced serial message not working in SENT decoder using IEP ECAP example PRU-IO 11.00.00 onwards -

Errata

ID Head Line Module SDK Status
i2189 OSPI: Controller PHY Tuning Algorithm OSPI Implemented
i2311 USART: Spurious DMA Interrupts UART Implemented
i2324 No synchronizer present between GCM and GCD status signals Common Implemented
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2351 OSPI: Controller does not support Continuous Read mode with NAND Flash OSPI Implemented
i2354 SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM Open
i2356 ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set ADC Implemented
i2375 SDFM: SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected SDFM Open
i2383 OSPI: 2-byte address is not supported in PHY DDR mode OSPI Implemented
i2479 OSPI Boot Issue with GPIO61 Reset Pin Configuration OSPI Open
i2480 1µs Glitch on GPIO61/OSPI0_RESET_OUT0 during OSPI Boot GPIO Open
i2404 Race condition in mailbox registers resulting in events miss IPC, Mailbox Implemented

Limitations

ID Head Line Module Reported in release Workaround
- DP83TG720-EVM-AM2 and DP83826-EVM-AM2 dont work simultaneously for switching traffic in AM261-LP Rev E1 and E2 boards Networking 10.00.00 onwards -
MCUSDK-13630 Cache should not be enabled at last 32B L2 Bank boundary Cache 10.01.00 Create MPU configurations for last 32B of each L2 Bank with Non Cached attribute
- LP-AM261 Out-of-box CPSW networking examples supports Rev-A board version seamlessly with DP83869 PHY. Networking 11.00.00 onwards To use LP-AM261 Rev-E1,Rev-E2 boards, follow the steps mentioned in Software modification needeed to use Rev-E1 and Rev-E2 version of LP-AM261 EVM.

Upgrade and Compatibility Information

LP / SOM Rev E2 to Rev A revision Changes

Component Change Comments
ADC / CMPSS ADC / CMPSS pin positions have changed in LP Rev A ADC0 Channels 0,4,6 have changed their pin positions from pins 23,26,29 in Rev E2 to 26,29,23 in Rev A respectively. Updated Example documentations
ADC Burst Mode EPWM
ADC SOC software
ADC Software Interleaved Averaging
SDFM SDFM Pin Positions have Changed in LP Rev A SDFM1 Clk0, D0 and D3 have changed their default positions from 18,12,43 in Rev E2 to 6,3,10 in Rev A respectively. Please follow the Pinmux configurations accordingly. Updated Example sysconfig and documentation for SDFM ECAP Loop Back Example .
IO Expander IO Expander Pins have changed in LP Rev A IO Expander at 0x21H has updated pins P0,P3,P4,P5 from CPSW/ICSS_BRD_CONN_DET1, MDIO/MDC_MUX_SEL1, MDIO/MDC_MUX_SEL2, CPSW/ICSS_BRD_CONN_DET2 in E2 to BP_MUX_SW_S6, BP_MUX_SW_S4, MDIO/MDC_MUX_SEL, BP_MUX_SW_S5 in REV A .
GPIO GPIO Interrupt Pin has changed in LP and SOM Rev A For Launchpad, the GPIO interrupt pin has changed from GPIO124 to GPIO5 in REV A. GPIO INT Crossbar has changed from GPIO_INT_XBAR_GPIO_0_BANK_INTR_7 to GPIO_INT_XBAR_GPIO_0_BANK_INTR_0 in REV A.
For SOM, the GPIO interrupt pin has changed from GPIO128 to GPIO120 in REV A. GPIO INT Crossbar has changed from GPIO_INT_XBAR_GPIO_0_BANK_INTR_8 to GPIO_INT_XBAR_GPIO_0_BANK_INTR_7 in REV A.
PMIC Resolved PMIC watchdog reset issue on LP Rev A

With the hardware fix for the PMIC watchdog reset issue in LP Rev A, the software workaround has been removed from all SBLs. For LP Rev E2 boards, the workaround is still required. Ensure the PMIC module is enabled in the SBL sysconfig.

Migration to 400 MHz in ZFG package

Component Change Comments
Clocktree Switching between 500 MHz and 400 MHz in ZFG package has changed. There are two variants available, catering to different R5F clock frequencies: 400 MHz and 500 MHz. The default variant is 500 MHz, but users can switch to the 400 MHz variant. This switching was earlier done through clock module in sysconfig but now it's done through Device View settings (Switching between 500 MHz and 400 MHz in ZFG package)

Compiling examples in MacOS machines

Currently the gmac library packaged within SDK is compiled using gcc darwin23.6.0 on Apple MAC. To build SDK examples on a different toolchain, recompile the gmac library by using these steps:

$ cd {SDK_PATH}/tools/boot/multicore-elf/c_modules/gmac
$ make all
  • A new library will be created inside mac/dist.
  • Rename this file to "gmac.arm64-apple-darwin.darwin.dylib".

RPRC Image format is Deprecated and Corresponding SBL's are also removed from SDK

RPRC image format is no longer supported and MCELF will be the only file format. Older SBL's and Cfg files which mapped to RPRC format are removed and replaced with MCELF variants. Below is the list of updated SBL's and Cfg files:

Deprecated SBL + CFG File Supported SBL + CFG File
SBL QSPI (default_sbl_qspi.cfg) SBL QSPI MULTICORE ELF (mcelf_sbl_qspi.cfg)
SBL UART SBL UART MULTICORE ELF
SBL SD (default_sbl_sd.cfg) SBL SD MULTICORE ELF (mcelf_sbl_sd.cfg)
SBL CAN (default_sbl_can.cfg) SBL CAN MULTICORE ELF (mcelf_sbl_can.cfg)
SBL CAN UNIFLASH (default_sbl_can_uniflash.cfg, default_sbl_can_uniflash_app.cfg) SBL CAN UNIFLASH MULTICORE ELF (mcelf_sbl_can_uniflash.cfg, mcelf_sbl_can_uniflash_app.cfg)

Please refer to the updated SDK example makefiles for Infra changes.

Flash Reset moved to SysCfg

Earlier, flash reset was done in board.c file within application which is now moved to SysCfg. If Flash reset logic needs to be added, please enable "Enable Flash Reset API" configurable in Flash module. This is by enabled out of box for all SDK Flash examples. For custom flash, define the flash reset API in application and add the API name to "Flash Reset Function" configurable.

Module clock configuration through Clock Tree

Previously our SDK had a mix of hardcoded clock configurations and limited configuration flexibility through sysconfig for the modules. With Clocktree, we now have a clear view of the entire clock tree with configurable components like PLL, DPLL, muxes, dividers added with validity checks. Earlier, the Input clock source and frequency for any module was configured through the module view in SysCfg. From now, this has to be done through clocktree.

Please refer to Clocktree for more details.

Migrating back from CCS Theia to CCS Eclipse

SDK was supporting CCS Eclipse until this release and now been migrated to support CCS Theia Out of Box. Below sections describe how to update the applications for Eclipse if needed.

Importing and Building in Eclipse

CCS Projectspec files are same for both Theia and Eclipse. Hence, no update is needed to import and build an SDK application on Eclipse.

CCS SBL Loading

JS Script for SBL loading on eclipse is updated to "load_sbl_eclipse.js". Please refer to CCS Tools for more details.

Migrating examples to 11.00.00 from older versions

Note
Images are shown for AM64x. It is application for AM261X as well.

Makefile Changes

Library Name change on makefile and CCS projects

From 11.00.00 SDK all the libraries are built separately for OS. There are separate libraries available for NoRTOS and FreeROTS. So the makefiles needs to be updated accordingly. Please refer the sample changes on the makefile below. These changes are not applicable for the libraries which were already built separately for NoRTOS/FreeRTOS like kernel libraries.

For NoRTOS/baremetal,

Library name change for NoRTOS example

For FreeRTOS,

Library name change for FreeRTOS example

similar change can be done on the CCS project as well

OS define on makefile and CCS projects

Additional macro OS_NORTOS or OS_FREERTOS should be defined on the makefile or CC project based on the OS of the project.

For NoRTOS/baremetal,

OS Macro addition for NoRTOS example

For FreeRTOS,

OS Macro addition for FreeRTOS example

SDL PBIST Self test

VIM Memory groups are added to PBIST self test from this release. Because of this change, Self test (SDL_PBIST_selfTest) API has to be called in polling mode only and interrupt mode is not supported.

Compiler Options

Module Affected API Change Additional Remarks
- - - -

SOC Device Drivers

Module Affected API Change Additional Remarks
- - - -

Networking

Module Affected API Change Additional Remarks
- - - -