AM261x MCU+ SDK  11.01.00
Release Notes 10.00.01

Attention
1. Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
2. There is a known issue of PMIC Watchdog resetting the SOC every 10 mins in CCS Gel flow. This has been fixed in SBL flow by disabling PMIC Watchdog using I2C interface. Use Flash SBL NULL if CCS Debug is needed or Add the same logic for PMIC Watchdog disable in application if CCS debug using Gel flow is mandatory.
3. Networking examples support has been tested only on AM261x-LP board.
4. SDK Datasheet is not generated for AM261x. This will be available in the next SDK release.
5. This is an early access release for AM261x SOM Board with limited testing to enable early development for customers. Basic validation of every IP has been done except Networking components and USB.
6. There is a known issue of OSPI Phy Tuning not working on AM261x LP and SOM Board. So, Phy tuning is disabled by default in Examples and SBL OSPI.
7. DFU Utils tool is not supported on Mac systems due to a build issue.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
SOM Board Basic Support SDK Infra
Derby PMIC Driver and Example support SDK Infra
Basic Ethernet MAC and Switch Support Networking
LwIP TCP/IP stack and gPTP TimeSync stack Networking
Auto PHY (DP83TG720-EVM-AM2) and Industrial PHY (DP83826-EVM-AM2) Support Networking

Modules Not tested/supported in this release

  • USB and Networking support on AM261x SOM Board.
  • OSPI Phy Tuning on AM261x LP and SOM Board.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM261x R5F AM261x Launchpad (referred to as am261x-lp in code).
Windows 10 64b or Ubuntu 18.04 64b or MacOS
AM261x R5F AM261x SOM (referred to as am261x-som in code).
Windows 10 64b or Ubuntu 18.04 64b or MacOS

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.8.1
SysConfig R5F 1.21.2 build, build 3837
TI ARM CLANG R5F 4.0.1.LTS
FreeRTOS Kernel R5F 11.1.0
LwIP R5F STABLE-2_2_0_RELEASE
Mbed-TLS R5F 2.13.1

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
- -

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: OSPI, UART. All R5F's. RPRC, multi-core image format Force Dual Core Mode

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Examples: adc_soc_continuous_dma, adc_alternate_dma_trigger Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA (normal and alternate triggers), EPWM trip through PPB limit, PPB features, Burst mode, Single and Differential mode, Interrupt with Offset from Aquisition Window, EPWM/ECAP/RTI triggered conversions, Trigger Repeater for Undersampling and Oversampling, Global Force on Multiple ADCs, Internal DAC Loopback to Calibration Channels, Safety Checker and Aggregator, Open Short Detection feature External channel selection
Bootloader R5F YES Yes. DMA enabled for SBL OSPI Boot modes: OSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip, digital filter, Calibration CMPSS Dac LoopBack feature
CPSW R5F YES No MAC & PHY loopback(DP83826-EVM-AM2) with RMII 100Mbps, MAC & PHY loopback(DP83TG720-EVM-AM2) with RGMII 1Gbps, LWIP (DP83TG720-EVM-AM2, DP83826-EVM-AM2): Getting IP, Ping, Layer 2 MAC, Layer 2 PTP Timestamping and Ethernet CPSW Switch support, TSN stack MII mode
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES yes. Example : ecap_edma ECAP APWM mode, PWM capture, DMA trigger in both APWM and Capture Modes, Signal Monitoring features -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Yes. Example: epwm_dma, epwm_xcmp_dma Multiple EPWM Sync from Top Module, PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, chopper module features, type5 features, global load and link feature -
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement, speed direction, cw-ccw modes -
FSI R5F YES YES RX, TX, polling, interrupt, DMA mode, single lane loopback. - FSI Spi Mode
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
LIN R5F YES YES RX, TX, polling, interrupt, DMA mode. -
MCAN R5F YES No RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode -
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
PINMUX R5F YES NA Tested with multiple peripheral pinmuxes -
PMU R5F NO NA Tested various PMU events Counter overflow detection is not enabled
OptiFlash R5F Yes NA FLC, RL2, RAT functionality, XIP with RL2 enabled OptiShare
OSPI R5F YES Yes. Example: ospi_flash_dma Read direct, Write indirect, Read/Write commands, DMA for read Phy Support
RTI R5F YES No Counter read, timebase selection, comparator setup for Interrupt, DMA requests Capture feature, fast enabling/disabling of events not tested
SDFM R5F YES No ECAP Clock LoopBack, Filter data read from CPU, Filter data read with PWM sync, triggered DMA read from the Filter FIFO -
SOC R5F YES NA Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation -
SPINLOCK R5F NA NA Lock, unlock HW spinlock -
UART R5F YES Yes. Example: uart_echo_dma Basic read/write at baud rate 115200, polling, interrupt mode HW flow control not tested, DMA mode not supported
WATCHDOG R5F YES NA Reset mode, Interrupt mode -

Trigonometric Operations

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
TMU R5F NO NA TMU Operations, Pipelining, Contex Save Square Root, Division Operations. more than 1 Interrupt Nesting for the contex save is not Supported.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
FLASH R5F YES OSPI Flash -
LED R5F YES GPIO -
ETHPHY R5F YES Tested with ethercat_slave_beckhoff_ssc_demo example -
IOEXPANDER R5F YES IO configurability -
PMIC R5F YES Watchdog Reset and disable -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Time-Sensitive Networking(gPTP-IEEE 802.1AS) R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, scatter-gather Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC & PHY loopback with RMII 100Mbps(DP83826-EVM-AM2), MAC & PHY loopback with RMII 100Mbps(DP83TG720-EVM-AM2), Layer 2 MAC, Packet Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer and Classifier MII mode
ICSS-EMAC R5F YES FreeRTOS Switch and MAC features, Storm Prevention (MAC), Host Statistics, Multicast Filtering Promiscuous Mode

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-13754 AM261x: Port 1 RX not working with DP83826-EVM-AM2 PHY Networking 10.00.00 onwards -
MCUSDK-13748 Am261x adc_soc_software_sync and adc_sw_interleaved_averaging example not working ADC 10.00.00 onwards -
MCUSDK-13748 ADC reference monitor instance doesn't match the refernece buffer instance ADC 10.00.00 onwards updated the monitor instances.
MCUSDK-13164 AM26x: EPWM DeadBand example failure EPWM 10.00.00 onwards phase shift adds a tbclk delay. added another EPWM instance to sync.
MCUSDK-13634 EPWM: Remove eventsUsed from Action Qualifier Syscfg. EPWM 10.00.00 onwards removed unused eventUsed element from the examples syscfg
MCUSDK-13747 EPWM DE example is failing due to incorrect pwmsyncoutxbar EPWM 10.00.00 onwards updated the pwmxbarsyncout cslr files.
MCUSDK-13670 SDFM ECAP loopback example used explicit HW_REG_RD SDFM 10.00.00 onwards updated the register read with corresponding API.
MCUSDK-13851 AM261x does not have support for UART4 and UART5. UART 10.00.00 AM261x Added UART4 and UART5 instance support in SysCfg.
MCUSDK-13773 EEPROM Read-Write not working properly. I2C 10.00.00 AM261x EEPROM Address was incorrect.

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-13865 HRPWM Deadband sfo example has 1ns jitter EPWM 10.00.00 onwards -
MCUSDK-13755 AM261x: 10% RX align code and CRC errors in port 2 Networking 10.00.00 onwards -
SMCUAPPS-972 AM261x: Gel files upgrade to program the HSDIVIDER clock correctly MCU Apps 10.00.01 onwards -
MCUSDK-13828 AM261x: ENET: Iperf TCP failing with 1Gbps Networking 10.00.01 onwards -
MCUSDK-13829 AM261x: ENET: EST fails for priority 0 with IND phy Networking 10.00.01 onwards -
MCUSDK-13836 Networking examples not working in SBL null and SBL OSPI boot mode SBL 10.00.01 onwards Load the image in DEV/CCS boot mode
MCUSDK-13847 AM261x: GPTP lwIP debug example doesnt fit in RAM Networking 10.00.01 onwards -
MCUSDK-13513 AM263Px, AM261x: UDP IPERF TX is unstable with 100Mbps link speed Networking 10.00.01 onwards -
MCUSDK-14052 AM261x: OSPI Phy tuning fails on am261x LP OSPI 10.00.00 onwards -
MCUSDK-14054 MMCSD: SysCfg sanity failure on AM26x devices MMCSD 10.00.01 onwards Use default configuration as in SDK examples.
MCUSDK-14055 SBL DFU and SBL DFU Uniflash Example failure USB 10.00.01 onwards -
MCUSDK-14056 Klocwork issues on USB Driver USB 10.00.01 onwards -
PINDSW-7715 Dual EMAC instance not working with both ports together for icss_emac_lwip example ICSS-EMAC 10.00.01 onwards None
PINDSW-7746 Low iperf values in TCP and UDP ICSS-EMAC 10.00.01 onwards None
PINDSW-8118 Enabling DHCP mode in icss_emac_lwip example causes assert ICSS-EMAC 10.00.01 onwards None
MCUSDK-13201 HRPWM waveform not generating (in updwon count) when prescaler is non-zero and HRPE is enabled EPWM 10.00.01 onwards None
MCUSDK-13834 EQEP: EQEP frequency measurement example is not working as expected EQEP 10.00.01 onwards None
- - - - -

Errata

ID Head Line Module SDK Status
- - - -

Limitations

ID Head Line Module Reported in release Workaround
- DP83TG720-EVM-AM2 and DP83826-EVM-AM2 dont work simultaneously for switching traffic in AM261-LP boards Networking 10.00.00 onwards -
- - - - -

Upgrade and Compatibility Information

Compiler Options

Module Affected API Change Additional Remarks
- - - -

SOC Device Drivers

Module Affected API Change Additional Remarks
ADC ADC_setupSOC updates to enumeration ADC_Channel The Channel 6 for the AM261x is present at "7" while the Cal Channel is present at "6"
- - - -

Networking

Module Affected API Change Additional Remarks
- - - -