AM261x MCU+ SDK  11.01.00
SDL TMU ROM_CHECKSUM Example

Introduction

This example demonstrates usage of the SDL TMU ROM Checksum. This example is used to check the integrity of the TMU ROM data. Its work is to take a set of data associated with the memory regions of TMU ROM and perform checksum on that data and then compare that resultant data value against a pre-determined golden vector value.

Use Cases

Use Case Description
UC-1 Calculate TMU ROM CHECKSUM from R5F Core.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss1-0 nortos
Toolchain ti-arm-clang
Board am261x-som
Example folder examples/sdl/tmu_rom_checksum/

Steps to Run the Example

See Also

TMU_ROM_CHECKSUM

Sample Output

TMU ROM Checksum Example Application
Calculating TMU ROM Checksum
TMU ROM-Checksum Data integrity passed
Calcuated TMU CRC High : 0xccdab254
Calcuated TMU CRC Low : 0x36cfb524
All tests Passed