AM261x MCU+ SDK  11.01.00
Optiflash XIP Benchmark with 32KB L2 Cache

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am261x-lp, am261x-som
Example folder examples/benchmarks/optiflash_benchmark/flash_xip_l2_cache_32k

Introduction

This is the same application as Optiflash OCRAM Benchmark, however, target functions are kept in external flash and L2 cache of 32KB is enabled. The effect of it is seen in the execution time.

Steps to Run the Example

Building the application

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Running the application

Flash the application binary to the device, follow the steps mentioned here (see Flash a Hello World example).

Sample output

Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 6 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init : 497us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 96us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 1us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 4475us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 3605us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 8us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 8684us
Image loading done, switching to application ...
OCMC benchmarking:: Board_init success
Filling up the buffers
master_task
master_task -- start sending
memcpy Exec Time I$ Miss I$ Acc INST ICM/sec INST/sec
0B 25457us 86576 1075457 2168807 4.2 105.2
100B 25227us 86072 1222264 2358034 4.2 115.4
200B 26261us 86573 1372107 2558131 4.1 120.3
400B 28200us 87814 1676802 2960263 3.8 129.6
700B 28158us 83225 2115467 3545671 3.7 155.5
1000B 30558us 85485 2578388 4160642 3.5 168.2
1500B 34107us 84059 3328963 5152837 3.0 186.6
2250B 40341us 87028 4471527 6667359 2.7 204.1
2500B 42833us 86446 4835914 7154867 2.5 206.3
4096B 53754us 86089 7236358 10350263 2.0 237.8
All tests have passed