AM261x MCU+ SDK  11.01.00
Optiflash XIP Benchmark with 16KB L2 Cache

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
Toolchain ti-arm-clang
Boards am261x-lp, am261x-som
Example folder examples/benchmarks/optiflash_benchmark/flash_xip_l2_cache_16k

Introduction

This is the same application as Optiflash OCRAM Benchmark, however, target functions are kept in external flash and L2 cache of 16KB is enabled. The effect of it is seen in the execution time.

Steps to Run the Example

Building the application

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Running the application

Flash the application binary to the device, follow the steps mentioned here (see Flash a Hello World example).

Sample output

Starting OSPI Bootloader ...
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
KPI_DATA: [BOOTLOADER_PROFILE] Boot Media Clock : 166.667 MHz
KPI_DATA: [BOOTLOADER_PROFILE] Boot Image Size : 6 KB
KPI_DATA: [BOOTLOADER_PROFILE] Cores present :
r5f0-0
KPI_DATA: [BOOTLOADER PROFILE] System_init : 497us
KPI_DATA: [BOOTLOADER PROFILE] Drivers_open : 96us
KPI_DATA: [BOOTLOADER PROFILE] LoadHsmRtFw : 1us
KPI_DATA: [BOOTLOADER PROFILE] Board_driversOpen : 4501us
KPI_DATA: [BOOTLOADER PROFILE] CPU load : 3607us
KPI_DATA: [BOOTLOADER PROFILE] SBL End : 8us
KPI_DATA: [BOOTLOADER_PROFILE] SBL Total Time Taken : 8712us
Image loading done, switching to application ...
OCMC benchmarking:: Board_init success
Filling up the buffers
master_task
master_task -- start sending
memcpy Exec Time I$ Miss I$ Acc INST ICM/sec INST/sec
0B 31201us 85983 1073886 2169476 3.4 85.9
100B 31901us 86247 1223635 2358979 3.3 91.3
200B 32214us 85832 1372983 2558957 3.3 98.1
400B 34200us 87916 1674185 2961071 3.2 106.9
700B 33988us 82973 2116351 3546487 3.0 128.9
1000B 36400us 85692 2579868 4161456 2.9 141.2
1500B 39516us 84308 3327332 5153546 2.6 161.1
2250B 45826us 86186 4470127 6667998 2.3 179.7
2500B 48070us 86331 4837108 7155812 2.2 183.8
4096B 59326us 85987 7234534 10351014 1.8 215.5
All tests have passed