AM261x MCU+ SDK  11.01.00
MPU Firewall Service DEMO

Introduction

This example demonstrates the use of HSM Firewall services.

2 services are available.

  1. Set Firewall Service is used to set firewall configuration.
  2. Set Firewall Interrupt service is responsible for the 4 operations mentioned below:
    • 2.1. Interrupt enable for protection and address violation
    • 2.2. Clearing Interrupt enable.
    • 2.3. Clearing Interrupt status.
    • 2.4. Clearing the current fault so that another can be captured.

Supported Combinations

Steps to Run the Example

Sample Output

On successful boot, following message will be seen on terminal. Please note that the R5F application has not been side-loaded yet.

[HSM_CLIENT] New Client Registered with Client Id = 0
Starting QSPI Bootloader ...
[BOOTLOADER_PROFILE] Boot Media : NOR SPI FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 80.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size : 28 KB
[BOOTLOADER_PROFILE] Cores present :
r5f0-1
r5f0-0
[BOOTLOADER PROFILE] System_init : 286us
[BOOTLOADER PROFILE] Drivers_open : 75us
[BOOTLOADER PROFILE] LoadHsmRtFw : 14503us
[BOOTLOADER PROFILE] Board_driversOpen : 2975us
[BOOTLOADER PROFILE] CPU load : 2292us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 20134us
Image loading done, switching to application ...
[HSM_CLIENT] New Client Registered with Client Id = 2
Enabling the interrupt for both address violation and protection violation for MPU_R5SS0_CORE1_AHB
Firewall request #1 status = 11111111 11111111
Permissions for peripheral region(0x52300000 - 0x523003FF) are revoked for R5FSS0_1
[HSM_CLIENT] New Client Registered with Client Id = 2
Interrupt registeration successful, notifying remote core to read CSL_UART0_U_BASE register
Success