AM261x MCU+ SDK  11.01.00
I2C Led Read Write LLD

Introduction

This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.

Application blinks leds for 3 loops in interrupt mode and 3 loops in polling mode. Application exits after 6 iterations.

Supported Combinations

Steps to Run the Example

See Also

I2C Low Level Driver

Sample Output

Shown below is a sample output when the application is run,

[I2C] LED Read Write Test Started ...
LED will Blink for 3 loop in polling Mode ...
LED will Blink for 3 loop in interrupt Mode ...
All tests have passed!!