AM261x MCU+ SDK  11.01.00
EDMA Polled Transfer

Introduction

This example demonstrates the data transfer using EDMA in polled mode

Supported Combinations

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[EDMA] Polled Transfer Test Started...
[EDMA] Polled Transfer Test Completed!!
All tests have passed!!