AM261x MCU+ SDK  11.01.00
DAC Random Voltage

Introduction

This example uses DAC to generate a Random Voltage on the DAC output.

The example does the below

  • Configures Timer to generate interrupt at a rate of 20KHz.
  • Assigns a Random value to a output variable and wirtes it to the Shadow Regester within the ISR.
  • This repeated programming of the registers generates a Random Votlage output.

External Connections

  • DAC output pin can be connected to an oscilloscope to view the Random Voltage output.

AM263X-CC or AM263PX-CC or AM261X-SOM E1

Note: To use the reference voltage generated on ControlCard, make sure that the System VREF source select switch on ControlCard is set to position 1-2

When using with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Capture waveform on HSEC Pin 9 (in case of AM261x and AM263Px please take care of IO expander)

AM263X-LP or AM263PX-LP

Note: To use the reference voltage generated on LaunchPad, make sure that the DAC_VREF source select switch S1 on LaunchPad is set to position 1-2

With AM263X-LP or AM263Px-LP

  • Capture the waveform on boosterpack header J1/J3 Pin 30

Supported Combinations

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Use an Oscilloscope to view the random voltage on DAC output pin.

See Also

DAC

Sample Output

Shown below is a sample output when the application is run,

DAC Random Voltage Test Started ...
DAC Random Voltage Test Passed!!
All tests have passed!!

Sample Output